Multicast entry type info apart from MAC address.
Data Fields | |
| bool | super |
| CpswAle_FwdStateLevel | fwdState |
| uint32_t | portMask |
| uint32_t | numIgnBits |
| bool CpswAle_McastEntryInfo::super |
Supervisory flag which indicates that this address can be received in port state other than Forwarding state
| CpswAle_FwdStateLevel CpswAle_McastEntryInfo::fwdState |
Forward state level
| uint32_t CpswAle_McastEntryInfo::portMask |
Port bit mask that is returned with a found multicast destination address
| uint32_t CpswAle_McastEntryInfo::numIgnBits |
Number of bits in the address to ignore. Up to 10 least significant bits can be ignored to form a multicast address range