Init time VLAN configuration.
Data Fields | |
| bool | aleVlanAwareMode |
| bool | cpswVlanAwareMode |
| bool | autoLearnWithVlan |
| bool | unknownVlanNoLearn |
| uint32_t | unknownForceUntaggedEgressMask |
| uint32_t | unknownRegMcastFloodMask |
| uint32_t | unknownUnregMcastFloodMask |
| uint32_t | unknownVlanMemberListMask |
| bool CpswAle_InitVlanCfg::aleVlanAwareMode |
Configure ALE to operate in VLAN aware mode
| bool CpswAle_InitVlanCfg::cpswVlanAwareMode |
Flag indicating if CPSW is in VLAN aware mode
| bool CpswAle_InitVlanCfg::autoLearnWithVlan |
Learn VLAN with address when autolearning addresses
| bool CpswAle_InitVlanCfg::unknownVlanNoLearn |
Do not learn addresses with unknown VLAN
| uint32_t CpswAle_InitVlanCfg::unknownForceUntaggedEgressMask |
Unknown VLAN Force Untagged Egress
| uint32_t CpswAle_InitVlanCfg::unknownRegMcastFloodMask |
Unknown VLAN Registered Multicast Flood Mask
| uint32_t CpswAle_InitVlanCfg::unknownUnregMcastFloodMask |
Unknown VLAN Multicast Flood Mask
| uint32_t CpswAle_InitVlanCfg::unknownVlanMemberListMask |
Unknown VLAN Member List