CSIRX Instance Object. Used internally, not to be used by end users.
Data Fields | |
bool | isOpen |
0: instance is not opened, 1: instance is open More... | |
CSIRX_ContextObject | context [CSIRX_CONTEXTS_MAX] |
Context specific state information. More... | |
uint32_t | startOfFrameIntr0ContextId |
NOT to used by end users. More... | |
uint32_t | startOfFrameIntr1ContextId |
NOT to used by end users. More... | |
uint32_t | endOfFrameIntr0ContextId |
NOT to used by end users. More... | |
uint32_t | endOfFrameIntr1ContextId |
NOT to used by end users. More... | |
CSIRX_CommonIntrCallbacks | intrCallbacks |
NOT to used by end users. More... | |
HwiP_Object | commonIntrObj |
NOT to used by end users. More... | |
HwiP_Object | combinedEndOfLineIntrObj |
NOT to used by end users. More... | |
HwiP_Object | combinedEndOfFrameIntrObj |
NOT to used by end users. More... | |
HwiP_Object | startOfFrameIntr0IntrObj |
NOT to used by end users. More... | |
HwiP_Object | startOfFrameIntr1IntrObj |
NOT to used by end users. More... | |
bool CSIRX_Object::isOpen |
0: instance is not opened, 1: instance is open
CSIRX_ContextObject CSIRX_Object::context[CSIRX_CONTEXTS_MAX] |
Context specific state information.
uint32_t CSIRX_Object::startOfFrameIntr0ContextId |
NOT to used by end users.
uint32_t CSIRX_Object::startOfFrameIntr1ContextId |
NOT to used by end users.
uint32_t CSIRX_Object::endOfFrameIntr0ContextId |
NOT to used by end users.
uint32_t CSIRX_Object::endOfFrameIntr1ContextId |
NOT to used by end users.
CSIRX_CommonIntrCallbacks CSIRX_Object::intrCallbacks |
NOT to used by end users.
HwiP_Object CSIRX_Object::commonIntrObj |
NOT to used by end users.
HwiP_Object CSIRX_Object::combinedEndOfLineIntrObj |
NOT to used by end users.
HwiP_Object CSIRX_Object::combinedEndOfFrameIntrObj |
NOT to used by end users.
HwiP_Object CSIRX_Object::startOfFrameIntr0IntrObj |
NOT to used by end users.
HwiP_Object CSIRX_Object::startOfFrameIntr1IntrObj |
NOT to used by end users.