CSIRX HW Attributes. Generated when using sysconfig.
Data Fields | |
uint32_t | csirxRegs |
CSIRX IP registers. More... | |
uint32_t | rcssCtrlRegs |
Additional CSIRX control registers, located in SOC top level CTRL regs. More... | |
uint32_t | hwInstId |
HW instance ID, 0: CSI2A, 1: CSI2B as so on. More... | |
uint32_t | ctrlClockHz |
CSI interface control clock in Hz. In AM723x, this is 96000000 Hz. More... | |
uint32_t | interconnectClockHz |
CSI interconnect control clock in Hz. In AM723x, this is 200000000 Hz. More... | |
uint16_t | commonIntNum |
CPU Interrupt number, if interrupt not connected, set to CSIRX_INTERRUPT_NOT_CONNECTED_ID. More... | |
uint16_t | combinedEndOfLineIntNum |
CPU Interrupt number, if interrupt not connected, set to CSIRX_INTERRUPT_NOT_CONNECTED_ID. More... | |
uint16_t | combinedEndOfFrameIntNum |
CPU Interrupt number, if interrupt not connected, set to CSIRX_INTERRUPT_NOT_CONNECTED_ID. More... | |
uint16_t | startOfFrameIntr0IntNum |
CPU Interrupt number, if interrupt not connected, set to CSIRX_INTERRUPT_NOT_CONNECTED_ID. More... | |
uint16_t | startOfFrameIntr1IntNum |
CPU Interrupt number, if interrupt not connected, set to CSIRX_INTERRUPT_NOT_CONNECTED_ID. More... | |
uint16_t | contextEndOfLineIntNum [CSIRX_CONTEXTS_MAX] |
CPU Interrupt number, if interrupt not connected, set to CSIRX_INTERRUPT_NOT_CONNECTED_ID. More... | |
uint32_t CSIRX_HwAttrs::csirxRegs |
CSIRX IP registers.
uint32_t CSIRX_HwAttrs::rcssCtrlRegs |
Additional CSIRX control registers, located in SOC top level CTRL regs.
uint32_t CSIRX_HwAttrs::hwInstId |
HW instance ID, 0: CSI2A, 1: CSI2B as so on.
uint32_t CSIRX_HwAttrs::ctrlClockHz |
CSI interface control clock in Hz. In AM723x, this is 96000000 Hz.
uint32_t CSIRX_HwAttrs::interconnectClockHz |
CSI interconnect control clock in Hz. In AM723x, this is 200000000 Hz.
uint16_t CSIRX_HwAttrs::commonIntNum |
CPU Interrupt number, if interrupt not connected, set to CSIRX_INTERRUPT_NOT_CONNECTED_ID.
uint16_t CSIRX_HwAttrs::combinedEndOfLineIntNum |
CPU Interrupt number, if interrupt not connected, set to CSIRX_INTERRUPT_NOT_CONNECTED_ID.
uint16_t CSIRX_HwAttrs::combinedEndOfFrameIntNum |
CPU Interrupt number, if interrupt not connected, set to CSIRX_INTERRUPT_NOT_CONNECTED_ID.
uint16_t CSIRX_HwAttrs::startOfFrameIntr0IntNum |
CPU Interrupt number, if interrupt not connected, set to CSIRX_INTERRUPT_NOT_CONNECTED_ID.
uint16_t CSIRX_HwAttrs::startOfFrameIntr1IntNum |
CPU Interrupt number, if interrupt not connected, set to CSIRX_INTERRUPT_NOT_CONNECTED_ID.
uint16_t CSIRX_HwAttrs::contextEndOfLineIntNum[CSIRX_CONTEXTS_MAX] |
CPU Interrupt number, if interrupt not connected, set to CSIRX_INTERRUPT_NOT_CONNECTED_ID.