DPHY configuration.
Data Fields | |
uint32_t | ddrClockInHz |
DDR clock speed in Hz. More... | |
bool | isClockMissingDetectionEnabled |
Set to true if wanting to enable clock missing detector. More... | |
uint8_t | triggerEscapeCode [4] |
Trigger escape codes. More... | |
uint32_t CSIRX_DphyConfig::ddrClockInHz |
DDR clock speed in Hz.
bool CSIRX_DphyConfig::isClockMissingDetectionEnabled |
Set to true if wanting to enable clock missing detector.
uint8_t CSIRX_DphyConfig::triggerEscapeCode[4] |
Trigger escape codes.