Transcoding configuration.
Data Fields | |
uint8_t | transcodeFormat |
Transcoding format, one of CSIRX_TRANSCODE_FORMAT. More... | |
bool | isHorizontalDownscalingBy2Enabled |
If true, horizontal down scaling by 2 is enabled, else disabled. More... | |
CSIRX_ContextCropConfig | crop |
Cropping configuration. More... | |
uint8_t CSIRX_ContextTranscodeConfig::transcodeFormat |
Transcoding format, one of CSIRX_TRANSCODE_FORMAT.
bool CSIRX_ContextTranscodeConfig::isHorizontalDownscalingBy2Enabled |
If true, horizontal down scaling by 2 is enabled, else disabled.
CSIRX_ContextCropConfig CSIRX_ContextTranscodeConfig::crop |
Cropping configuration.