CBUFF Software Triggered Session configuration.
The structure describes the configuration required to be specified if the session is created in software triggered mode.
Data Fields | |
CBUFF_BufferCfg | userBufferInfo [CBUFF_MAX_USER_BUFFER] |
User supplied data buffers which can be transmitted over the interface. More... | |
CBUFF_BufferCfg CBUFF_SwSessionCfg::userBufferInfo[CBUFF_MAX_USER_BUFFER] |
User supplied data buffers which can be transmitted over the interface.