CBUFF LVDS Initialization configuration.
The structure describes the configuration which is required to configure the LVDS
Data Fields | |
uint8_t | crcEnable |
Enable/Disable CRC on LVDS. More... | |
uint8_t | lvdsLaneEnable |
LVDS Lane configuration: The bit mask here is used to indicate the active LVDS lanes i.e. Bit 0 implies Lane-0, Bit 1 implies Lanel-1 etc. More... | |
uint8_t | msbFirst |
Set the flag to 1 to indicate that the MSB is sent first or LSB. More... | |
uint8_t | ddrClockMode |
Set the flag to 1 for DDR Clock Mode and 0 for SDR. More... | |
uint8_t | ddrClockModeMux |
Set the flag to 1 for DDR Mode Clock Mux and 0 for SDR Mode Clock Mux. More... | |
CBUFF_LVDSLaneFmtMap | laneFormat |
LVDS Lane Format: More... | |
uint8_t CBUFF_LVDSCfg::crcEnable |
Enable/Disable CRC on LVDS.
uint8_t CBUFF_LVDSCfg::lvdsLaneEnable |
LVDS Lane configuration: The bit mask here is used to indicate the active LVDS lanes i.e. Bit 0 implies Lane-0, Bit 1 implies Lanel-1 etc.
The number of LVDS lanes is platform specific and is defined in the CBUFF platform file.
uint8_t CBUFF_LVDSCfg::msbFirst |
Set the flag to 1 to indicate that the MSB is sent first or LSB.
uint8_t CBUFF_LVDSCfg::ddrClockMode |
Set the flag to 1 for DDR Clock Mode and 0 for SDR.
uint8_t CBUFF_LVDSCfg::ddrClockModeMux |
Set the flag to 1 for DDR Mode Clock Mux and 0 for SDR Mode Clock Mux.
CBUFF_LVDSLaneFmtMap CBUFF_LVDSCfg::laneFormat |
LVDS Lane Format: