CBUFF EDMA Tracking Entry.
The structure holds information about the EDMA channel which has been added to correspond to the linked list entry to DMA the data into the CBUFF.
Data Fields | |
CBUFF_EDMAChannelCfg | cbuffEDMAChannelCfg |
EDMA Channel Configuration allocated by the application and which is used to program the CBUFF Transfers. More... | |
uint32_t | srcAddress |
Source address of the EDMA Transfer. More... | |
uint32_t | transferSize |
Size of the data being transferred by the EDMA. This is stored in CBUFF Units. More... | |
CBUFF_EDMAChannelCfg CBUFF_EDMATrackingEntry::cbuffEDMAChannelCfg |
EDMA Channel Configuration allocated by the application and which is used to program the CBUFF Transfers.
uint32_t CBUFF_EDMATrackingEntry::srcAddress |
Source address of the EDMA Transfer.
uint32_t CBUFF_EDMATrackingEntry::transferSize |
Size of the data being transferred by the EDMA. This is stored in CBUFF Units.