CBUFF instance attributes - used during init time.
Data Fields | |
uint32_t | baseAddr |
uint32_t | fifoBaseAddr |
uint32_t | maxLVDSLanesSupported |
uint32_t | errorIntrNum |
uint32_t | intrNum |
uint32_t | cbuffChannelId [CBUFF_MAX_NUM_SESSION] |
uint32_t CBUFF_Attrs::baseAddr |
Peripheral base address
uint32_t CBUFF_Attrs::fifoBaseAddr |
ADCBUF base address
uint32_t CBUFF_Attrs::maxLVDSLanesSupported |
Max LVDS Lines supported
uint32_t CBUFF_Attrs::errorIntrNum |
Error Interrupt Number
uint32_t CBUFF_Attrs::intrNum |
Interrupt Number
uint32_t CBUFF_Attrs::cbuffChannelId[CBUFF_MAX_NUM_SESSION] |
CBUFF EDMA Physical Channel Identifier: