![Logo](ti_logo.svg) |
AM273x MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
35 #ifndef SDL_STC_SOC_H_
36 #define SDL_STC_SOC_H_
38 #include <sdl/include/am273x/sdlr_soc_baseaddress.h>
39 #include <sdl/include/am273x/sdlr_mss_rcm.h>
40 #include <sdl/include/am273x/sdlr_mss_ctrl.h>
41 #include <sdl/include/am273x/sdlr_dss_rcm.h>
42 #include <sdl/include/am273x/sdlr_dss_ctrl.h>
70 #define SDL_STC_NUM_INSTANCES 2U
72 #define SDL_DSP_PD_WAKEUP_MASK0_WAKEUP_MASK0 (0xEFFFFFFFU)
121 #define MSS_RCM_BaseAddress (SDL_MSS_RCM_U_BASE)
122 #define MSS_CTRL_BaseAddress (SDL_MSS_CTRL_U_BASE)
126 #define DSS_RCM_BaseAddress (SDL_DSS_RCM_U_BASE)
127 #define DSS_CTRL_BaseAddress (SDL_DSS_CTRL_U_BASE)
128 #define DSS_DSP_ICFG_PDCCMD (0x01810000U)
@ SDL_STC_INST_MAINR5F0
Definition: sdl_stc_soc.h:85
SDL_STC_Inst
Definition: sdl_stc_soc.h:83
static void SDL_STC_resetCauseClear(void)
This API is used to clear the reset cause bits for processor core.
@ INVALID_INSTANCE
Definition: sdl_stc_soc.h:88
@ SDL_STC_INST_DSP
Definition: sdl_stc_soc.h:86
#define SDL_STC_NUM_INSTANCES
Definition: sdl_stc_soc.h:70
static uint32_t SDL_STC_baseAddress[SDL_STC_NUM_INSTANCES]
Definition: sdl_stc_soc.h:119