|
AM273x MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
42 #ifndef SDL_SOC_CCM_H_
43 #define SDL_SOC_CCM_H_
48 #include <sdl/include/am273x/sdlr_soc_baseaddress.h>
50 #include <sdl/esm/soc/am273x/sdl_esm_core.h>
51 #include <sdl/include/am273x/sdlr_intr_esm_mss.h>
59 #define SDL_ESM_INSTANCE_MSS (SDL_ESMG1_CCMR5_ST_ERR)
60 #define SDL_INTR_GROUP_NUM 1U
61 #define SDL_INTR_GROUP_NUMBER 2U
62 #define BASEADDRESS SDL_MSS_CCMR_U_BASE
63 #define ESM_INSTANCE SDL_ESM_INST_MSS_ESM
65 #define SDL_INTR_PRIORITY_LVL 1U
66 #define SDL_ENABLE_ERR_PIN 1U
67 #define SDL_ESM_MAX_EVENT_MAP_NUM 2u
75 #define SDL_MSS_CCMR 0U
77 #define SDL_CCM_MAX_INSTANCE 1U
Header file contains enumerations, structure definitions and function declarations for SDL Error Sign...
static uint32_t SDL_CCM_baseAddress[SDL_CCM_MAX_INSTANCE]
This API is used to get the base address of the instance.
Definition: sdl_soc_ccm.h:85
int32_t SDL_ESM_CCMapplicationCallback(SDL_ESM_Inst esmInstType, int32_t grpChannel, int32_t intSrc, void *arg)
#define SDL_CCM_MAX_INSTANCE
Definition: sdl_soc_ccm.h:77
This file contains the macro definations for Register layer.
uint32_t SDL_CCM_Inst
CCM Instance supported.
Definition: sdl_soc_ccm.h:73