Go to the source code of this file.
Enumerations | |
| enum | SDL_MCRC_InstType { DSS_MCRC = 1, MSS_MCRC = 2, SDL_MCRC_INVALID = 0xffff } |
| MCRC Instance supported. More... | |
Functions | |
| int32_t | SDL_MCRC_getBaseaddr (SDL_MCRC_InstType instance, uint32_t *baseAddr) |
| This API is used to get the base address of the instance. More... | |