Go to the source code of this file.
Macros | |
| #define | SDL_HWA_CFG (uint32_t)SDL_DSS_HWA_CFG_U_BASE |
| #define | SDL_HWA_BUS_CFG (uint32_t)SDL_DSS_CTRL_U_BASE |
| #define | SDL_HWA_DMA0_ADDRESS (uint32_t)SDL_DSS_HWA_DMA0_U_BASE |
| #define | SDL_HWA_DMA1_ADDRESS (uint32_t)SDL_DSS_HWA_DMA1_U_BASE |
| #define SDL_HWA_CFG (uint32_t)SDL_DSS_HWA_CFG_U_BASE |
| #define SDL_HWA_BUS_CFG (uint32_t)SDL_DSS_CTRL_U_BASE |
| #define SDL_HWA_DMA0_ADDRESS (uint32_t)SDL_DSS_HWA_DMA0_U_BASE |
| #define SDL_HWA_DMA1_ADDRESS (uint32_t)SDL_DSS_HWA_DMA1_U_BASE |