QSPI Driver API/interface file.
Go to the source code of this file.
| Data Structures | |
| struct | QSPI_Transaction | 
| Data structure used with QSPI_Transfers - QSPI_writeConfigMode, QSPI_readMemMapMode.  More... | |
| struct | QSPI_ReadCmdParams | 
| struct | QSPI_WriteCmdParams | 
| struct | QSPI_Params | 
| QSPI Parameters.  More... | |
| struct | QSPI_Object | 
| QSPI driver object.  More... | |
| struct | QSPI_Attrs | 
| QSPI instance attributes - used during init time.  More... | |
| struct | QSPI_Config | 
| Macros | |
| Macros for invalid commands | |
| #define | QSPI_CMD_INVALID_OPCODE (0xFFU) | 
| #define | QSPI_CMD_INVALID_ADDR (0xFFFFFFFFU) | 
| Transfer Status Code | |
| #define | QSPI_TRANSFER_COMPLETED (0U) | 
| #define | QSPI_TRANSFER_STARTED (1U) | 
| #define | QSPI_TRANSFER_CANCELLED (2U) | 
| #define | QSPI_TRANSFER_FAILED (3U) | 
| #define | QSPI_TRANSFER_CSN_DEASSERT (4U) | 
| #define | QSPI_TRANSFER_TIMEOUT (5U) | 
| Typedefs | |
| typedef void * | QSPI_Handle | 
| A handle that is returned from a QSPI_open() call.  More... | |
| Functions | |
| void | QSPI_init (void) | 
| This function initializes the QSPI module.  More... | |
| void | QSPI_deinit (void) | 
| This function de-initializes the QSPI module.  More... | |
| void | QSPI_Params_init (QSPI_Params *qspiParams) | 
| Initialize data structure with defaults.  More... | |
| QSPI_Handle | QSPI_open (uint32_t index, const QSPI_Params *openParams) | 
| This function opens a given QSPI peripheral.  More... | |
| void | QSPI_close (QSPI_Handle handle) | 
| Function to close a QSPI peripheral specified by the QSPI handle.  More... | |
| QSPI_Handle | QSPI_getHandle (uint32_t index) | 
| This function returns the handle of an open QSPI Instance from the instance index.  More... | |
| uint32_t | QSPI_getInputClk (QSPI_Handle handle) | 
| This function returns the input clock at which QSPI was programmed.  More... | |
| void | QSPI_transaction_init (QSPI_Transaction *trans) | 
| Function to initialize the QSPI_Transaction structure.  More... | |
| void | QSPI_readCmdParams_init (QSPI_ReadCmdParams *rdParams) | 
| Function to initialize the QSPI_Transaction structure.  More... | |
| void | QSPI_writeCmdParams_init (QSPI_WriteCmdParams *wrParams) | 
| Function to initialize the QSPI_Transaction structure.  More... | |
| int32_t | QSPI_setPreScaler (QSPI_Handle handle, uint32_t clkDividerVal) | 
| Set the QSPI clock register divider value.  More... | |
| int32_t | QSPI_setWriteCmd (QSPI_Handle handle, uint8_t command) | 
| Function to set write command to be used.  More... | |
| int32_t | QSPI_setReadCmd (QSPI_Handle handle, uint8_t command) | 
| Function to set read command to be used.  More... | |
| int32_t | QSPI_setAddressByteCount (QSPI_Handle handle, uint32_t count) | 
| Function to set number of address bytes to be used.  More... | |
| int32_t | QSPI_setDummyBitCount (QSPI_Handle handle, uint32_t count) | 
| Function to set number of dummy bits to be used.  More... | |
| int32_t | QSPI_setMemAddrSpace (QSPI_Handle handle, uint32_t memMappedPortSwitch) | 
| This function is used to switch between memory mapped and configuration mode.  More... | |
| int32_t | QSPI_intEnable (QSPI_Handle handle, uint32_t intFlag) | 
| This function is used to enable word or frame complete interrupt.  More... | |
| int32_t | QSPI_intDisable (QSPI_Handle handle, uint32_t intFlag) | 
| This function is used to disable word or frame complete interrupt.  More... | |
| int32_t | QSPI_intClear (QSPI_Handle handle, uint32_t intFlag) | 
| This function is used to clear word or frame complete interrupt.  More... | |
| int32_t | QSPI_setRxLines (QSPI_Handle handle, uint32_t rxLines) | 
| Set QSPI Rx lines in the QSPI object.  More... | |
| uint32_t | QSPI_getRxLines (QSPI_Handle handle) | 
| Get QSPI Rx lines in the QSPI object.  More... | |
| void | OSPI_phyGetTuningData (uint32_t *phyTuningData, uint32_t *phyTuningDataSize) | 
| Different QSPI Transfer functions | |
| int32_t | QSPI_readMemMapMode (QSPI_Handle handle, QSPI_Transaction *trans) | 
| Function to perform reads from the flash in memory mapped mode.  More... | |
| int32_t | QSPI_writeCmd (QSPI_Handle handle, QSPI_WriteCmdParams *wrParams) | 
| Function to send specific commands and related data to flash.  More... | |
| int32_t | QSPI_writeConfigMode (QSPI_Handle handle, const QSPI_Transaction *trans) | 
| Function to perform writes to the flash in configuration mode.  More... | |
| int32_t | QSPI_writeConfigModeIntr (QSPI_Handle handle, QSPI_WriteCmdParams *wrParams) | 
| Function to perform write to the flash in interrupt mode mode.  More... | |
| int32_t | QSPI_readCmd (QSPI_Handle handle, QSPI_ReadCmdParams *rdParams) | 
| Function to send specific commands and receive related data from flash.  More... | |
| int32_t | QSPI_readConfigModeIntr (QSPI_Handle handle, QSPI_ReadCmdParams *rdParams) | 
| Function to perform read from the flash in interrupt mode.  More... | |
| Variables | |
| QSPI_Config | gQspiConfig [] | 
| Externally defined driver configuration array.  More... | |
| uint32_t | gQspiConfigNum | 
| Externally defined driver configuration array size.  More... | |
| QSPI_EdmaParams | gqspiEdmaParam | 
| EDMA Paramter for QSPI Transaction.  More... | |