![Logo](ti_logo.svg) |
AM273x MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
56 #include "sdl_hwa_hw.h"
58 #include <sdl/hwa/v0/soc/sdl_hwa_soc.h>
59 #include <sdl/esm/sdlr_esm.h>
60 #if defined (SOC_AM273X)
62 #include <sdl/include/am273x/sdlr_intr_esm_dss.h>
63 #include <sdl/include/am273x/sdlr_intr_esm_mss.h>
64 #elif defined (SOC_AWR294X)
66 #include <sdl/include/awr294x/sdlr_intr_esm_dss.h>
67 #include <sdl/include/awr294x/sdlr_intr_esm_mss.h>
92 #define SDL_HWA_INIT_TIMEOUT (0XFFU)
Header file contains enumerations, structure definitions and function declarations for SDL Error Sign...
This file contains the prototypes of the APIs present in the device abstraction layer file of HWA....
SDL_HWA_MemBlock
Definition: sdl_ip_hwa.h:108
SDL_HWA_MemID
Definition: sdl_ip_hwa.h:133
int32_t SDL_HWA_memParityExecute(SDL_HWA_MemID memID, SDL_HWA_MemBlock memBlock)
This API is used for configuring and testing parity of the HWA memory.
int32_t SDL_HWA_ESM_CallbackFunction(SDL_ESM_Inst instance, int32_t grpChannel, int32_t vecNum, void *arg)
This API is a call back function when an interrupt is occured for HWA memory parity and fsm Lockstep.
int32_t SDL_HWA_fsmLockStepExecute(void)
This API is used to induce the error in the fsm lockstep for HWA.