Functions | |
int32_t | SDL_HWA_ESM_CallbackFunction (SDL_ESM_Inst instance, int32_t grpChannel, int32_t vecNum, void *arg) |
This API is a call back function when an interrupt is occured for HWA memory parity and fsm Lockstep. More... | |
int32_t | SDL_HWA_memParityExecute (SDL_HWA_MemID memID, SDL_HWA_MemBlock memBlock) |
This API is used for configuring and testing parity of the HWA memory. More... | |
int32_t | SDL_HWA_fsmLockStepExecute (void) |
This API is used to induce the error in the fsm lockstep for HWA. More... | |
int32_t SDL_HWA_ESM_CallbackFunction | ( | SDL_ESM_Inst | instance, |
int32_t | grpChannel, | ||
int32_t | vecNum, | ||
void * | arg | ||
) |
This API is a call back function when an interrupt is occured for HWA memory parity and fsm Lockstep.
instance | indicates the ESM instance |
grpChannel | indicates the ESM channel number for HWA memory parity and fsm Lockstep |
vecNum | indicates the ESM vector number for HWA memory parity and fsm Lockstep |
arg | pointer to input arrguments |
int32_t SDL_HWA_memParityExecute | ( | SDL_HWA_MemID | memID, |
SDL_HWA_MemBlock | memBlock | ||
) |
This API is used for configuring and testing parity of the HWA memory.
memID | indicates the memory in the HWA |
memBlock | indicates the memory block in the HWA memory |
int32_t SDL_HWA_fsmLockStepExecute | ( | void | ) |
This API is used to induce the error in the fsm lockstep for HWA.