AM273x MCU+ SDK  09.02.00

Introduction

This module contains APIs to program and use the DTHE.

Files

file  dthe.h
 This file contains the prototype of DTHE driver APIs.
 

Data Structures

struct  DTHE_Attrs
 DTHE attributes. More...
 
struct  DTHE_Config
 DTHE driver context. More...
 

Functions

void DTHE_init (void)
 This function initializes the DTHE. More...
 
void DTHE_deinit (void)
 This function de-initializes the DTHE. More...
 
DTHE_Handle DTHE_open (uint32_t index)
 Function to open DTHE instance, enable DTHE engine. More...
 
DTHE_Return_t DTHE_close (DTHE_Handle handle)
 Function to close a DTHE module specified by the DTHE handle. More...
 

Typedefs

typedef void * DTHE_Handle
 Handle to the DTHE driver. More...
 

Enumerations

enum  DTHE_Return_t { DTHE_RETURN_SUCCESS = 0xCE50311AU, DTHE_RETURN_FAILURE = 0x924FC5E7U }
 DTHE Driver Error code. More...
 

Typedef Documentation

◆ DTHE_Handle

typedef void* DTHE_Handle

Handle to the DTHE driver.

Enumeration Type Documentation

◆ DTHE_Return_t

DTHE Driver Error code.

The enumeration describes all the possible return and error codes which the DTHE Driver can return

Enumerator
DTHE_RETURN_SUCCESS 

Success/pass return code

DTHE_RETURN_FAILURE 

General or unspecified failure/error

Function Documentation

◆ DTHE_init()

void DTHE_init ( void  )

This function initializes the DTHE.

◆ DTHE_deinit()

void DTHE_deinit ( void  )

This function de-initializes the DTHE.

◆ DTHE_open()

DTHE_Handle DTHE_open ( uint32_t  index)

Function to open DTHE instance, enable DTHE engine.

Parameters
indexIndex of config to use in the DTHE_Config array.
Returns
A DTHE_Handle on success or a NULL on an error.

◆ DTHE_close()

DTHE_Return_t DTHE_close ( DTHE_Handle  handle)

Function to close a DTHE module specified by the DTHE handle.

Parameters
handleDTHE_Handle returned from DTHE_open()
Returns
DTHE_RETURN_SUCCESS if requested operation completed. DTHE_RETURN_FAILURE if requested operation not completed.

Variable Documentation

◆ gDtheConfig

DTHE_Config gDtheConfig[]
extern

Externally defined driver configuration array.

◆ gDtheConfigNum

uint32_t gDtheConfigNum
extern

Externally defined driver configuration Num.