Functions | |
uint32_t | SDL_r5fGetResetCause (void) |
Get R5 reset cause. More... | |
void | SDL_generateSwWarmReset (void) |
Generate SW WARM reset. More... | |
uint32_t | SDL_getWarmResetCause (void) |
Returns cause of WARM reset. More... | |
void | SDL_rcmDspLocalReset (void) |
Reset Dsp Core. More... | |
uint32_t SDL_r5fGetResetCause | ( | void | ) |
Get R5 reset cause.
void SDL_generateSwWarmReset | ( | void | ) |
Generate SW WARM reset.
uint32_t SDL_getWarmResetCause | ( | void | ) |
Returns cause of WARM reset.
void SDL_rcmDspLocalReset | ( | void | ) |
Reset Dsp Core.