AM273x MCU+ SDK  09.02.00

Introduction

Functions

int32_t SDL_ECC_BUS_SAFETY_DSS_secExecute (uint32_t busSftyNode, uint32_t addr, uint32_t wr_data)
 This API is used for SEC test on DSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_DSS_dedExecute (uint32_t busSftyNode, uint32_t addr, uint32_t wr_data)
 This API is used for DED test on DSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_DSS_redExecute (uint32_t busSftyNode, SDL_ECC_BUS_SAFETY_busSftyFiType fiType, SDL_ECC_BUS_SAFETY_busSftyFiRedType redType)
 This API is used for RED test on DSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_DSS_secErrorClear (uint32_t busSftyNode)
 This API is used to clear SEC error on DSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_DSS_getSecErrorStatus (uint32_t busSftyNode, uint32_t *status)
 This API is used to get SEC error Status on DSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_DSS_dedErrorClear (uint32_t busSftyNode)
 This API is used to clear DED error on DSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_DSS_getDedErrorStatus (uint32_t busSftyNode, uint32_t *status)
 This API is used to get DED error Status on DSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_DSS_redErrorClear (uint32_t busSftyNode)
 This API is used to clear RED error on DSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_DSS_getRedErrorStatus (uint32_t busSftyNode, uint32_t *status)
 This API is used to get RED error Status on DSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_DSS_readStaticRegs (uint32_t busSftyNode, SDL_ECC_BUS_SAFETY_staticRegs *pStaticRegs)
 This API is used to get DSS static register values. More...
 
int32_t SDL_ECC_BUS_SAFETY_MSS_secExecute (uint32_t busSftyNode, uint32_t addr, uint32_t wr_data)
 This API is used for SEC test on MSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_MSS_dedExecute (uint32_t busSftyNode, uint32_t addr, uint32_t wr_data)
 This API is used for DED test on MSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_MSS_redExecute (uint32_t busSftyNode, SDL_ECC_BUS_SAFETY_busSftyFiType fiType, SDL_ECC_BUS_SAFETY_busSftyFiRedType redType)
 This API is used for RED test on MSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_MSS_secErrorClear (uint32_t busSftyNode)
 This API is used to clear SEC error on MSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_MSS_getSecErrorStatus (uint32_t busSftyNode, uint32_t *status)
 This API is used to get SEC error Status on MSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_MSS_dedErrorClear (uint32_t busSftyNode)
 This API is used to clear DED error on MSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_MSS_getDedErrorStatus (uint32_t busSftyNode, uint32_t *status)
 This API is used to get DED error Status on MSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_MSS_redErrorClear (uint32_t busSftyNode)
 This API is used to clear RED error on MSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_MSS_getRedErrorStatus (uint32_t busSftyNode, uint32_t *status)
 This API is used to get RED error Status on MSS. More...
 
int32_t SDL_ECC_BUS_SAFETY_MSS_readStaticRegs (uint32_t busSftyNode, SDL_ECC_BUS_SAFETY_staticRegs *pStaticRegs)
 This API is used to get MSS static register values. More...
 
uint32_t SDL_ECC_BUS_SAFETY_DSS_AWR2944_AWR2943_Detect (void)
 This API is used to detect the device AWR2944/ Awr2943. More...
 

Function Documentation

◆ SDL_ECC_BUS_SAFETY_DSS_secExecute()

int32_t SDL_ECC_BUS_SAFETY_DSS_secExecute ( uint32_t  busSftyNode,
uint32_t  addr,
uint32_t  wr_data 
)

This API is used for SEC test on DSS.

Parameters
busSftyNodeNode identifier
addraddress to which data to be written
wr_datadata to be be written on the address
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_DSS_dedExecute()

int32_t SDL_ECC_BUS_SAFETY_DSS_dedExecute ( uint32_t  busSftyNode,
uint32_t  addr,
uint32_t  wr_data 
)

This API is used for DED test on DSS.

Parameters
busSftyNodeNode identifier
addraddress to which data to be written
wr_datadata to be be written on the address
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_DSS_redExecute()

int32_t SDL_ECC_BUS_SAFETY_DSS_redExecute ( uint32_t  busSftyNode,
SDL_ECC_BUS_SAFETY_busSftyFiType  fiType,
SDL_ECC_BUS_SAFETY_busSftyFiRedType  redType 
)

This API is used for RED test on DSS.

Parameters
busSftyNodeNode identifier
fiTypeindicates the Fi type
redTypeindicates interface type
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_DSS_secErrorClear()

int32_t SDL_ECC_BUS_SAFETY_DSS_secErrorClear ( uint32_t  busSftyNode)

This API is used to clear SEC error on DSS.

Parameters
busSftyNodeNode identifier
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_DSS_getSecErrorStatus()

int32_t SDL_ECC_BUS_SAFETY_DSS_getSecErrorStatus ( uint32_t  busSftyNode,
uint32_t *  status 
)

This API is used to get SEC error Status on DSS.

Parameters
busSftyNodeNode identifier
statuspointer to which status to be updated
Returns
status return the Test status. SDL_PASS: success

◆ SDL_ECC_BUS_SAFETY_DSS_dedErrorClear()

int32_t SDL_ECC_BUS_SAFETY_DSS_dedErrorClear ( uint32_t  busSftyNode)

This API is used to clear DED error on DSS.

Parameters
busSftyNodeNode identifier
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_DSS_getDedErrorStatus()

int32_t SDL_ECC_BUS_SAFETY_DSS_getDedErrorStatus ( uint32_t  busSftyNode,
uint32_t *  status 
)

This API is used to get DED error Status on DSS.

Parameters
busSftyNodeNode identifier
statuspointer to which status to be updated
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_DSS_redErrorClear()

int32_t SDL_ECC_BUS_SAFETY_DSS_redErrorClear ( uint32_t  busSftyNode)

This API is used to clear RED error on DSS.

Parameters
busSftyNodeNode identifier
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments SDL_EFAIL: failure, indicate verify failed

◆ SDL_ECC_BUS_SAFETY_DSS_getRedErrorStatus()

int32_t SDL_ECC_BUS_SAFETY_DSS_getRedErrorStatus ( uint32_t  busSftyNode,
uint32_t *  status 
)

This API is used to get RED error Status on DSS.

Parameters
busSftyNodeNode identifier
statuspointer to which status to be updated
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_DSS_readStaticRegs()

int32_t SDL_ECC_BUS_SAFETY_DSS_readStaticRegs ( uint32_t  busSftyNode,
SDL_ECC_BUS_SAFETY_staticRegs pStaticRegs 
)

This API is used to get DSS static register values.

Parameters
busSftyNodeNode identifier
pStaticRegspointer to staic register
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_MSS_secExecute()

int32_t SDL_ECC_BUS_SAFETY_MSS_secExecute ( uint32_t  busSftyNode,
uint32_t  addr,
uint32_t  wr_data 
)

This API is used for SEC test on MSS.

Parameters
busSftyNodeNode identifier
addraddress to which data to be written
wr_datadata to be be written on the address
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_MSS_dedExecute()

int32_t SDL_ECC_BUS_SAFETY_MSS_dedExecute ( uint32_t  busSftyNode,
uint32_t  addr,
uint32_t  wr_data 
)

This API is used for DED test on MSS.

Parameters
busSftyNodeNode identifier
addraddress to which data to be written
wr_datadata to be be written on the address
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_MSS_redExecute()

int32_t SDL_ECC_BUS_SAFETY_MSS_redExecute ( uint32_t  busSftyNode,
SDL_ECC_BUS_SAFETY_busSftyFiType  fiType,
SDL_ECC_BUS_SAFETY_busSftyFiRedType  redType 
)

This API is used for RED test on MSS.

Parameters
busSftyNodeNode identifier
fiTypeindicates the Fi type
redTypeindicates interface type
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_MSS_secErrorClear()

int32_t SDL_ECC_BUS_SAFETY_MSS_secErrorClear ( uint32_t  busSftyNode)

This API is used to clear SEC error on MSS.

Parameters
busSftyNodeNode identifier
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_MSS_getSecErrorStatus()

int32_t SDL_ECC_BUS_SAFETY_MSS_getSecErrorStatus ( uint32_t  busSftyNode,
uint32_t *  status 
)

This API is used to get SEC error Status on MSS.

Parameters
busSftyNodeNode identifier
statuspointer to which status to be updated
Returns
status return the Test status. SDL_PASS: success

◆ SDL_ECC_BUS_SAFETY_MSS_dedErrorClear()

int32_t SDL_ECC_BUS_SAFETY_MSS_dedErrorClear ( uint32_t  busSftyNode)

This API is used to clear DED error on MSS.

Parameters
busSftyNodeNode identifier
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_MSS_getDedErrorStatus()

int32_t SDL_ECC_BUS_SAFETY_MSS_getDedErrorStatus ( uint32_t  busSftyNode,
uint32_t *  status 
)

This API is used to get DED error Status on MSS.

Parameters
busSftyNodeNode identifier
statuspointer to which status to be updated
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_MSS_redErrorClear()

int32_t SDL_ECC_BUS_SAFETY_MSS_redErrorClear ( uint32_t  busSftyNode)

This API is used to clear RED error on MSS.

Parameters
busSftyNodeNode identifier
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments SDL_EFAIL: failure, indicate verify failed

◆ SDL_ECC_BUS_SAFETY_MSS_getRedErrorStatus()

int32_t SDL_ECC_BUS_SAFETY_MSS_getRedErrorStatus ( uint32_t  busSftyNode,
uint32_t *  status 
)

This API is used to get RED error Status on MSS.

Parameters
busSftyNodeNode identifier
statuspointer to which status to be updated
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_MSS_readStaticRegs()

int32_t SDL_ECC_BUS_SAFETY_MSS_readStaticRegs ( uint32_t  busSftyNode,
SDL_ECC_BUS_SAFETY_staticRegs pStaticRegs 
)

This API is used to get MSS static register values.

Parameters
busSftyNodeNode identifier
pStaticRegspointer to staic register
Returns
status return the Test status. SDL_PASS: success SDL_EBADARGS: failure, indicate the bad input arguments

◆ SDL_ECC_BUS_SAFETY_DSS_AWR2944_AWR2943_Detect()

uint32_t SDL_ECC_BUS_SAFETY_DSS_AWR2944_AWR2943_Detect ( void  )

This API is used to detect the device AWR2944/ Awr2943.

Returns
status returns status to detect awr2943 or awr2944 soc