This file contains the top-level API of the Enet driver.
Go to the source code of this file.
Functions | |
| uint32_t | Enet_getCoreId (void) |
| EnetTrace_TraceLevel | Enet_setTraceLevel (EnetTrace_TraceLevel level) |
| Set global trace level. More... | |
| EnetTrace_TraceLevel | Enet_getTraceLevel (void) |
| Get current trace level. More... | |
| void | Enet_initOsalCfg (EnetOsal_Cfg *osalCfg) |
| Initialize OSAL configuration. More... | |
| void | Enet_initUtilsCfg (EnetUtils_Cfg *utilsCfg) |
| Initialize utils configuration. More... | |
| void | Enet_init (const EnetOsal_Cfg *osalCfg, const EnetUtils_Cfg *utilsCfg) |
| Initialize Enet LLD. More... | |
| void | Enet_deinit (void) |
| De-initialize Enet LLD. More... | |
| Enet_Handle | Enet_getHandle (Enet_Type enetType, uint32_t instId) |
| Get the Enet handle of a peripheral. More... | |
| uint32_t | Enet_getMacPortMax (Enet_Type enetType, uint32_t instId) |
| Get number of MAC ports available in the Ethernet peripheral. More... | |
| void | Enet_initCfg (Enet_Type enetType, uint32_t instId, void *cfg, uint32_t cfgSize) |
| Initialize the peripheral configuration parameters. More... | |
| Enet_Handle | Enet_open (Enet_Type enetType, uint32_t instId, const void *cfg, uint32_t cfgSize) |
| Open and initializes the Enet driver for a peripheral. More... | |
| Enet_Handle | Enet_rejoin (Enet_Type enetType, uint32_t instId) |
| Rejoin a running Ethernet peripheral. More... | |
| EnetDma_Handle | Enet_getDmaHandle (Enet_Handle hEnet) |
| Get the handle to the DMA used for packet transmit/receive. More... | |
| void | Enet_registerEventCb (Enet_Handle hEnet, Enet_Event evt, uint32_t evtNum, Enet_EventCallback evtCb, void *evtCbArgs) |
| Register a callback for an event. More... | |
| void | Enet_unregisterEventCb (Enet_Handle hEnet, Enet_Event evt, uint32_t evtNum) |
| Unregister callback for an event. More... | |
| void | Enet_poll (Enet_Handle hEnet, Enet_Event evt, const void *arg, uint32_t argSize) |
| Poll for Ethernet events. More... | |
| void | Enet_periodicTick (Enet_Handle hEnet) |
| Run periodic tick on the Ethernet peripheral. More... | |
| uint32_t | Enet_getMacPortCnt (Enet_Handle hEnet) |
| Get number of MAC ports available in the Ethernet peripheral. More... | |
| void | Enet_close (Enet_Handle hEnet) |
| Close the Enet peripheral. More... | |
| int32_t | Enet_saveCtxt (Enet_Handle hEnet) |
| Save and closes the context of the Enet peripheral. More... | |
| int32_t | Enet_restoreCtxt (Enet_Type enetType, uint32_t instId) |
| Restore and open the context of the Enet peripheral. More... | |
| int32_t | Enet_hardResetCpsw (Enet_Handle hEnet, Enet_Type enetType, uint32_t instId, Enet_notify_t *pCpswTriggerResetCb) |
| Hard reset CPSW peripheral. More... | |
| int32_t | Enet_getHandleInfo (Enet_Handle hEnet, Enet_Type *enetType, uint32_t *instId) |
| Get enetType and instId info from the enet handle. More... | |