This file contains the type definitions and helper macros for the CPSW Statistics module interface.
Go to the source code of this file.
Data Structures | |
| struct | CpswStats_HostPort_2g |
| CPSW 2G host port statistics. More... | |
| struct | CpswStats_MacPort_2g |
| CPSW 2G MAC port statistics. More... | |
| struct | CpswStats_HostPort_Ng |
| CPSW 5G or 9G host port statistics. More... | |
| struct | CpswStats_MacPort_Ng |
| CPSW 5G or 9G MAC port statistics. More... | |
| struct | CpswStats_PortStats |
| CPSW nG port statistics. More... | |
Macros | |
| #define | CPSW_STATS_BLOCK_ELEM_NUM (128U) |
| Number of elements in a statistics block. More... | |