Introduction
This example demonstrates the usage of the SDL HWA module.
The example shows how to setup and use the Parity and FSM Lockstep Diagnostic operation. Shows the generation of parity and FSM Lockstep errors on HWA data memory
Use Cases
Use Case | Description |
UC-1 | Parity insertion on HWA DMA0 DMEM0. |
UC-2 | Parity insertion on HWA DMA0 DMEM1. |
UC-3 | Parity insertion on HWA DMA0 DMEM2. |
UC-4 | Parity insertion on HWA DMA0 DMEM3. |
UC-5 | Parity insertion on HWA DMA0 DMEM4. |
UC-6 | Parity insertion on HWA DMA0 DMEM5. |
UC-7 | Parity insertion on HWA DMA0 DMEM6. |
UC-8 | Parity insertion on HWA DMA0 DMEM7. |
UC-9 | Parity insertion on HWA DMA0 WindowRam. |
UC-10 | Parity insertion on HWA DMA1 DMEM0. |
UC-11 | Parity insertion on HWA DMA1 DMEM1. |
UC-12 | Parity insertion on HWA DMA1 DMEM2. |
UC-13 | Parity insertion on HWA DMA1 DMEM3. |
UC-14 | Parity insertion on HWA DMA1 DMEM4. |
UC-15 | Parity insertion on HWA DMA1 DMEM5. |
UC-16 | Parity insertion on HWA DMA1 DMEM6. |
UC-17 | Parity insertion on HWA DMA1 DMEM7. |
UC-18 | Parity insertion on HWA DMA1 WindowRam. |
UC-19 | FSM locstep insertion on HWA. |
Supported Combinations
Steps to Run the Example
See Also
HWA
Sample Output
Shown below is a sample output when the application is run,
[C66xx_DSP]
HWA Application
HWA TEST START : starting
ESM Initialization for all the SDL HWA Nodes is Done
Applications Name: HWA_ParityDMA0DMEM0Test PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA0DMEM1Test PASSED and Time taken for the Test is 16 micro secs
Applications Name: HWA_ParityDMA0DMEM2Test PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA0DMEM3Test PASSED and Time taken for the Test is 16 micro secs
Applications Name: HWA_ParityDMA0DMEM4Test PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA0DMEM5Test PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA0DMEM6Test PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA0DMEM7Test PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA0WindowRamTest PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA1DMEM0Test PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA1DMEM1Test PASSED and Time taken for the Test is 16 micro secs
Applications Name: HWA_ParityDMA1DMEM2Test PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA1DMEM3Test PASSED and Time taken for the Test is 16 micro secs
Applications Name: HWA_ParityDMA1DMEM4Test PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA1DMEM5Test PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA1DMEM6Test PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA1DMEM7Test PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_ParityDMA1WindowRamTest PASSED and Time taken for the Test is 17 micro secs
Applications Name: HWA_FsmLockStepTest PASSED and Time taken for the Test is 9 micro secs
All tests have passed