AM273x MCU+ SDK  09.01.00
EVM Setup

AM273X EVM

Cable Connections

  • The figure below shows some important cable connections, ports and switches.
    • Take note of the location of the "BOOTMODE" switch, this is used to switch between different boot modes like OSPI, UART, SD, NOBOOT mode

AM273X-EVM

Setup UART Terminal

  • Many examples use a standard UART terminal to log the output from the examples. You can use any UART terminal program for the same. Below steps show how to setup the UART terminal from CCS.
  • First identify the UART port as enumerated on the host machine.
    • Make sure that the EVM and UART cable connected as shown in Cable Connections
    • In windows, you can use the "Device Manager" to see the detected UART ports
      • Search "Device Manager" in Windows Search Box in the Windows taskbar.
    • If dont see any USB serial ports listed in "Device Manager" under "Ports (COM & LPT)", then make sure you have installed the UART to USB driver from FTDI, https://www.ftdichip.com/FTDrivers.htm.

Identify UART Port in Windows Device Manager
  • In CCS, goto "View > Terminal"

UART Terminal Menu
  • Open a new UART terminal

Open New UART Terminal
  • Select the UART port, keep other options to default, i.e 115200 baud rate - 8 data bits - No parity - 1 stop bit,
  • UART for R5F console is only visible in Device Manager when USB XDS110 cable is connected to EVM
  • UART for C66x console is only visible in Device Manager when UART to USB cable is connected to EVM
    • We use the 1st USB serial port, as seen in the device manager, when USB XDS110 cable is connected for below in the SDK
      • Flashing application via UART
      • Booting application via UART
      • Console output for examples which run from R5F
    • We use the 3rd USB serial port out of 4 ports emulated, when UART to USB cable is connected for below in the SDK
      • Console output for examples which run from C66x
    • In this screenshot this happens to be COM13 and COM14 however on your machine this could be different.
    • Tips for checking the right UART port number
      • disconnect all other UART to USB devices other than this EVM before checking in device manager.
      • un-plug and re-plug the USB FTDI and XDS110 connection to the PC while the Device Manager is open and the COM ports are visible

BOOT MODE

UART BOOT MODE

This mode is used to flash files to the EVM flash via UART. It can also be used to boot applications via UART.

SOP0 - Short
SOP2 - Short
SOP1 - Open

UART BOOT MODE

QSPI BOOT MODE

This mode is used to boot flashed applications via EVM flash like OSPI flash

SOP0 - Short
SOP2 - Open
SOP1 - Open

QSPI BOOT MODE

NOBOOT MODE

This mode is used with the Gel files without using the SBL.

SOP0 - Short
SOP2 - Open
SOP1 - Short

NO BOOT MODE