AM273x MCU+ SDK  08.06.00

Detailed Description

This structure contains the different configuration used for PBIST for the failure insertion test to generate negative result.


Design: PROC_SDL-977


Data Fields

uint32_t CA0
 
uint32_t CA1
 
uint32_t CA2
 
uint32_t CA3
 
uint32_t CL0
 
uint32_t CL1
 
uint32_t CL2
 
uint32_t CL3
 
uint32_t CMS
 
uint32_t CSR
 
uint32_t I0
 
uint32_t I1
 
uint32_t I2
 
uint32_t I3
 
uint32_t RAMT
 

Field Documentation

◆ CA0

uint32_t SDL_PBIST_configNeg::CA0

Failure insertion value for CA0 Value for the Failure Insertion Test Vector CA0

◆ CA1

uint32_t SDL_PBIST_configNeg::CA1

Failure insertion value for CA1 Value for the Failure Insertion Test Vector CA1

◆ CA2

uint32_t SDL_PBIST_configNeg::CA2

Failure insertion value for CA2 Value for the Failure Insertion Test Vector CA2

◆ CA3

uint32_t SDL_PBIST_configNeg::CA3

Failure insertion value for CA3 Value for the Failure Insertion Test Vector CA3

◆ CL0

uint32_t SDL_PBIST_configNeg::CL0

Failure insertion value for CL0 Value for the Failure Insertion Test Vector CL0

◆ CL1

uint32_t SDL_PBIST_configNeg::CL1

Failure insertion value for CL1 Value for the Failure Insertion Test Vector CL1

◆ CL2

uint32_t SDL_PBIST_configNeg::CL2

Failure insertion value for CL2 Value for the Failure Insertion Test Vector CL2

◆ CL3

uint32_t SDL_PBIST_configNeg::CL3

Failure insertion value for CL3 Value for the Failure Insertion Test Vector CL3

◆ CMS

uint32_t SDL_PBIST_configNeg::CMS

Failure insertion value for CMS Value for the Failure Insertion Test Vector CMS

◆ CSR

uint32_t SDL_PBIST_configNeg::CSR

Failure insertion value for CSR Value for the Failure Insertion Test Vector CSR

◆ I0

uint32_t SDL_PBIST_configNeg::I0

Failure insertion value for I0 Value for the Failure Insertion Test Vector I0

◆ I1

uint32_t SDL_PBIST_configNeg::I1

Failure insertion value for I1 Value for the Failure Insertion Test Vector I1

◆ I2

uint32_t SDL_PBIST_configNeg::I2

Failure insertion value for I2 Value for the Failure Insertion Test Vector I2

◆ I3

uint32_t SDL_PBIST_configNeg::I3

Failure insertion value for I3 Value for the Failure Insertion Test Vector I3

◆ RAMT

uint32_t SDL_PBIST_configNeg::RAMT

Failure insertion value for RAMT Value for the Failure Insertion Test Vector RAMT