AM273x MCU+ SDK  08.06.00

Detailed Description

QSPI Parameters.

QSPI Parameters are used to with the QSPI_open() call. Default values for these parameters are set using QSPI_Params_init().

If NULL is passed for the parameters, QSPI_open() uses default parameters.

See also
QSPI_Params_init()

Data Fields

uint32_t edmaInst
 

Field Documentation

◆ edmaInst

uint32_t QSPI_Params::edmaInst

EDMA instance used for QSPI transfer