AM273x MCU+ SDK  08.06.00
MIBSPI_PeripheralModeParams Struct Reference

Detailed Description

MIBSPI peripheral mode Parameters.

MIBSPI peripheral Parameters are used with the MIBSPI_open() call when mode is set to MIBSPI_PERIPHERAL. Default values for these parameters are set using MIBSPI_Params_init().

See also
MIBSPI_Params_init()

Data Fields

uint32_t dmaReqLine
 
uint8_t chipSelect
 

Field Documentation

◆ dmaReqLine

uint32_t MIBSPI_PeripheralModeParams::dmaReqLine

DMA request line to be used for Peripheral

◆ chipSelect

uint8_t MIBSPI_PeripheralModeParams::chipSelect

CS0-CS7 signal number from 0 -7