Flash device config. This will be part of the flash config, so has to be filled by sysconfig or otherwise before invoking Flash_open.
Data Fields | |
uint8_t | cmdExtType |
uint8_t | byteOrder |
uint8_t | enable4BAddr |
uint8_t | addrByteSupport |
uint8_t | fourByteAddrEnSeq |
uint8_t | cmdWren |
uint8_t | cmdRdsr |
uint8_t | srWip |
uint8_t | srWel |
uint8_t | resetType |
uint8_t | deviceBusyType |
uint8_t | xspiWipRdCmd |
uint32_t | xspiWipReg |
uint32_t | xspiWipBit |
uint32_t | flashWriteTimeout |
uint32_t | flashBusyTimeout |
FlashCfg_EraseConfig | eraseCfg |
FlashCfg_ReadIDConfig | idCfg |
FlashCfg_ProtoEnConfig | protocolCfg |
uint8_t Flash_DevConfig::cmdExtType |
uint8_t Flash_DevConfig::byteOrder |
uint8_t Flash_DevConfig::enable4BAddr |
uint8_t Flash_DevConfig::addrByteSupport |
uint8_t Flash_DevConfig::fourByteAddrEnSeq |
uint8_t Flash_DevConfig::cmdWren |
uint8_t Flash_DevConfig::cmdRdsr |
uint8_t Flash_DevConfig::srWip |
uint8_t Flash_DevConfig::srWel |
uint8_t Flash_DevConfig::resetType |
uint8_t Flash_DevConfig::deviceBusyType |
uint8_t Flash_DevConfig::xspiWipRdCmd |
uint32_t Flash_DevConfig::xspiWipReg |
uint32_t Flash_DevConfig::xspiWipBit |
uint32_t Flash_DevConfig::flashWriteTimeout |
uint32_t Flash_DevConfig::flashBusyTimeout |
FlashCfg_EraseConfig Flash_DevConfig::eraseCfg |
FlashCfg_ReadIDConfig Flash_DevConfig::idCfg |
FlashCfg_ProtoEnConfig Flash_DevConfig::protocolCfg |