AM273x MCU+ SDK  08.06.00
sdl_stc_soc.h File Reference

Go to the source code of this file.

Macros

#define SDL_STC_NUM_INSTANCES   2U
 
#define SDL_DSP_PD_WAKEUP_MASK0_WAKEUP_MASK0   (0xEFFFFFFFU)
 
#define MSS_RCM_BaseAddress   (SDL_MSS_RCM_U_BASE)
 
#define MSS_CTRL_BaseAddress   (SDL_MSS_CTRL_U_BASE)
 
#define DSS_RCM_BaseAddress   (SDL_DSS_RCM_U_BASE)
 
#define DSS_CTRL_BaseAddress   (SDL_DSS_CTRL_U_BASE)
 
#define DSS_DSP_ICFG_PDCCMD   (0x01810000U)
 

Enumerations

enum  SDL_STC_Inst { SDL_STC_INST_MAINR5F0, SDL_STC_INST_DSP, INVALID_INSTANCE }
 

Functions

static void SDL_STC_resetCauseClear (void)
 This API is used to clear the reset cause bits for processor core. More...
 

Variables

static uint32_t SDL_STC_baseAddress [SDL_STC_NUM_INSTANCES] = {SDL_MSS_R5SS_STC_U_BASE, SDL_DSS_DSP_STC_U_BASE}
 

Macro Definition Documentation

◆ SDL_STC_NUM_INSTANCES

#define SDL_STC_NUM_INSTANCES   2U

◆ SDL_DSP_PD_WAKEUP_MASK0_WAKEUP_MASK0

#define SDL_DSP_PD_WAKEUP_MASK0_WAKEUP_MASK0   (0xEFFFFFFFU)

◆ MSS_RCM_BaseAddress

#define MSS_RCM_BaseAddress   (SDL_MSS_RCM_U_BASE)

◆ MSS_CTRL_BaseAddress

#define MSS_CTRL_BaseAddress   (SDL_MSS_CTRL_U_BASE)

◆ DSS_RCM_BaseAddress

#define DSS_RCM_BaseAddress   (SDL_DSS_RCM_U_BASE)

◆ DSS_CTRL_BaseAddress

#define DSS_CTRL_BaseAddress   (SDL_DSS_CTRL_U_BASE)

◆ DSS_DSP_ICFG_PDCCMD

#define DSS_DSP_ICFG_PDCCMD   (0x01810000U)

Enumeration Type Documentation

◆ SDL_STC_Inst

Enumerator
SDL_STC_INST_MAINR5F0 
SDL_STC_INST_DSP 
INVALID_INSTANCE 

Variable Documentation

◆ SDL_STC_baseAddress

uint32_t SDL_STC_baseAddress[SDL_STC_NUM_INSTANCES] = {SDL_MSS_R5SS_STC_U_BASE, SDL_DSS_DSP_STC_U_BASE}
static