AM273x MCU+ SDK  08.06.00
sdl_hwa_soc.h File Reference

Go to the source code of this file.

Macros

#define SDL_HWA_CFG   (uint32_t)SDL_DSS_HWA_CFG_U_BASE
 
#define SDL_HWA_BUS_CFG   (uint32_t)SDL_DSS_CTRL_U_BASE
 
#define SDL_HWA_DMA0_ADDRESS   (uint32_t)SDL_DSS_HWA_DMA0_U_BASE
 
#define SDL_HWA_DMA1_ADDRESS   (uint32_t)SDL_DSS_HWA_DMA1_U_BASE
 

Macro Definition Documentation

◆ SDL_HWA_CFG

#define SDL_HWA_CFG   (uint32_t)SDL_DSS_HWA_CFG_U_BASE

◆ SDL_HWA_BUS_CFG

#define SDL_HWA_BUS_CFG   (uint32_t)SDL_DSS_CTRL_U_BASE

◆ SDL_HWA_DMA0_ADDRESS

#define SDL_HWA_DMA0_ADDRESS   (uint32_t)SDL_DSS_HWA_DMA0_U_BASE

◆ SDL_HWA_DMA1_ADDRESS

#define SDL_HWA_DMA1_ADDRESS   (uint32_t)SDL_DSS_HWA_DMA1_U_BASE