AM273x MCU+ SDK  08.06.00

Introduction

This file contains the prototypes of the APIs present in the device abstraction layer file of RESET. This also contains some related macros.

Go to the source code of this file.

Enumerations

SOC Warm Reset Causes

enum  SDL_SOC_WarmResetCause {
  SDL_WarmResetCause_POWER_ON_RESET = 0x09U, SDL_WarmResetCause_MSS_WDT = 0x0AU, SDL_WarmResetCause_TOP_RCM_WARM_RESET_CONFIG = 0x0CU, SDL_WarmResetCause_EXT_PAD_RESET = 0x08U,
  SDL_WarmResetCause_HSM_WDT = 0x18U
}
 

Functions

uint32_t SDL_r5fGetResetCause (void)
 Get R5 reset cause. More...
 
void SDL_generateSwWarmReset (void)
 Generate SW WARM reset. More...
 
uint32_t SDL_getWarmResetCause (void)
 Returns cause of WARM reset. More...
 
void SDL_rcmDspLocalReset (void)
 Reset Dsp Core. More...