===========================================================================
@{
◆ SDL_DCC_MODE_SINGLE_SHOT
Stop counting when counter0 and valid0 both reach zero
◆ SDL_DCC_MODE_CONTINUOUS
< Stop counting when counter1 reaches zero Continuously repeat (until error)
◆ SDL_DCC_CLK0_SRC_CLOCK0_0
SYS_CLK1 is selected as source for COUNT0
◆ SDL_DCC_CLK0_SRC_CLOCK0_1
SYS_CLK2 is selected as source for COUNT0
◆ SDL_DCC_CLK0_SRC_CLOCK0_2
XREF_CLK is selected as source for COUNT0
◆ SDL_DCC_CLK1_SRC_CLOCKSRC0
TEST_CLK0 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC1
TEST_CLK1 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC2
TEST_CLK2 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC3
TEST_CLK3 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC4
TEST_CLK4 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC5
TEST_CLK5 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC6
TEST_CLK6 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_CLOCKSRC7
TEST_CLK7 is selected as source for COUNT1
◆ SDL_DCC_CLK1_SRC_FICLK
OTHER_CLK is selected as source for COUNT1
◆ SDL_DCC_INTERRUPT_ERR
#define SDL_DCC_INTERRUPT_ERR (0x0U) |
◆ SDL_DCC_INTERRUPT_DONE
#define SDL_DCC_INTERRUPT_DONE (0x1U) |
◆ SDL_DCC_mode
Enum to select the DCC Operation Mode.
DCC can either operate in single shot or continuous mode.
◆ SDL_DCC_clkSrc0
Enum to select the COUNT0 clock source.
◆ SDL_DCC_clkSrc1
Enum to select the COUNT1 clock source.
◆ SDL_DCC_intrType
◆ SDL_STC_TestResult
Enumerator |
---|
SDL_STC_COMPLETED_SUCCESS | The STC completed and the test passed
|
SDL_STC_COMPLETED_FAILURE | The STC completed and the test failed
|
SDL_STC_NOT_COMPLETED | The STC was active but could not be completed.
|
SDL_STC_NOT_RUN | The STC was not performed on this device
|
INVALID_RESULT | The STC was not performed on this device
|
◆ SDL_STC_TestType
Enumerator |
---|
SDL_STC_TEST | The STC test should be completed and the test passed for this testType
|
SDL_STC_NEG_TEST | The STC test should be completed and the test failed for this testType
|
INVALID_TEST | |