Macros that define values for the shuffled addressing mode.
Macros | |
#define | HWA_SRC_SHUFFLE_AB_MODE_DISABLE ((uint8_t)0U) /** 0-disable */ |
#define | HWA_SRC_SHUFFLE_AB_MODE_ADIM ((uint8_t)1U) /** 1-SHUFFLE_LUT is used for sample index re-ordering in A dimension */ |
#define | HWA_SRC_SHUFFLE_AB_MODE_BDIM ((uint8_t)2U) /** 2- SHUFFLE_LUT is used in B-dimension */ |
#define HWA_SRC_SHUFFLE_AB_MODE_DISABLE ((uint8_t)0U) /** 0-disable */ |
#define HWA_SRC_SHUFFLE_AB_MODE_ADIM ((uint8_t)1U) /** 1-SHUFFLE_LUT is used for sample index re-ordering in A dimension */ |
#define HWA_SRC_SHUFFLE_AB_MODE_BDIM ((uint8_t)2U) /** 2- SHUFFLE_LUT is used in B-dimension */ |