Macros that define values for the destination of interrupt (CPU or DMA) when the paramset is completed. The interrupt type HWA_PARAMDONE_INTERRUPT_TYPE_CPU may not be supported on all versions of the IP - see HWA_Attrs::isConcurrentAccessAllowed.
Macros | |
#define | HWA_PARAMDONE_INTERRUPT_TYPE_CPU_INTR1 ((uint8_t)1U) |
#define | HWA_PARAMDONE_INTERRUPT_TYPE_CPU_INTR2 ((uint8_t)2U) |
#define | HWA_PARAMDONE_INTERRUPT_TYPE_DMA ((uint8_t)4U) |
#define HWA_PARAMDONE_INTERRUPT_TYPE_CPU_INTR1 ((uint8_t)1U) |
CPU Interrupt 1 when paramset is completed
#define HWA_PARAMDONE_INTERRUPT_TYPE_CPU_INTR2 ((uint8_t)2U) |
CPU Interrupt 2 when paramset is completed
#define HWA_PARAMDONE_INTERRUPT_TYPE_DMA ((uint8_t)4U) |
Trigger DMA when paramset is completed