Macros that define values for CFAR Noise Averaging mode.
Macros | |
#define | HWA_NOISE_AVG_MODE_CFAR_CA ((uint8_t)0U) |
#define | HWA_NOISE_AVG_MODE_CFAR_CAGO ((uint8_t)1U) |
#define | HWA_NOISE_AVG_MODE_CFAR_CASO ((uint8_t)2U) |
#define | HWA_NOISE_AVG_MODE_CFAR_OS ((uint8_t)3U) |
#define HWA_NOISE_AVG_MODE_CFAR_CA ((uint8_t)0U) |
cumulative average of left+right
#define HWA_NOISE_AVG_MODE_CFAR_CAGO ((uint8_t)1U) |
cumulative average of the side (left or right) that is greater
#define HWA_NOISE_AVG_MODE_CFAR_CASO ((uint8_t)2U) |
cumulative average of the side (left or right) that is smaller
#define HWA_NOISE_AVG_MODE_CFAR_OS ((uint8_t)3U) |
CFAR OS