Macros that define values for the complex multiply block with LUT based frequency de-rotation mode, set the RAM index incremented mode after each iteration, either auto-increment mode, in which the ram index is incremented automatically after each iteration, with either saturates at 63 or wraps around, or non-increment mode, in which the ram index is constant for all iterations,.
◆ HWA_LUT_FREQ_DEROTATE_RAMIDX_AUTOINCR_WRAPAROUND
#define HWA_LUT_FREQ_DEROTATE_RAMIDX_AUTOINCR_WRAPAROUND ((uint8_t)0U) /** auto-increment mode, with wrap around */ |
◆ HWA_LUT_FREQ_DEROTATE_RAMIDX_AUTOINCR_SATURATED
#define HWA_LUT_FREQ_DEROTATE_RAMIDX_AUTOINCR_SATURATED ((uint8_t)1U) /** auto-increment mode, with saturates at 63 */ |
◆ HWA_LUT_FREQ_DEROTATE_RAMIDX_NONINCR
#define HWA_LUT_FREQ_DEROTATE_RAMIDX_NONINCR ((uint8_t)2U) /** non-increment mode */ |