Macros that define values to enable and disable for detection threshold comparison.
Macros | |
#define | HWA_LOCALMAX_THRESH_BITMASK_BOTH_EN ((uint8_t)0U) |
#define | HWA_LOCALMAX_THRESH_BITMASK_CDIM_EN ((uint8_t)1U) |
#define | HWA_LOCALMAX_THRESH_BITMASK_BDIM_EN ((uint8_t)2U) |
#define | HWA_LOCALMAX_THRESH_BITMASK_BOTH_DIS ((uint8_t)3U) |
#define HWA_LOCALMAX_THRESH_BITMASK_BOTH_EN ((uint8_t)0U) |
enable CUT comparison with detection threshold in both dimensions
#define HWA_LOCALMAX_THRESH_BITMASK_CDIM_EN ((uint8_t)1U) |
enable CUT comparison with detection threshold in row dimension only (C-dimension threshold)
#define HWA_LOCALMAX_THRESH_BITMASK_BDIM_EN ((uint8_t)2U) |
enable CUT comparison with detection threshold in column dimension only(B-dimension)
#define HWA_LOCALMAX_THRESH_BITMASK_BOTH_DIS ((uint8_t)3U) |
disable CUT comparison with detection threshold in both dimensions