Macros that define values for the complex multiply block with FFT stitching mode. Useful for 4K and 8K FFT calculation, set the last 2 bits in TWIDINCR register, the rest 12 bits should be set to 0.
Macros | |
#define | HWA_FFT_STITCHING_TWID_PATTERN_4K ((uint8_t)1U) /** 4K fft stitching twid factor pattern */ |
#define | HWA_FFT_STITCHING_TWID_PATTERN_8K ((uint8_t)2U) /** 8K fft stitching twid factor pattern */ |
#define HWA_FFT_STITCHING_TWID_PATTERN_4K ((uint8_t)1U) /** 4K fft stitching twid factor pattern */ |
#define HWA_FFT_STITCHING_TWID_PATTERN_8K ((uint8_t)2U) /** 8K fft stitching twid factor pattern */ |