Macros that define values for the various outputs of the FFT block.
Macros | |
#define | HWA_FFT_MODE_OUTPUT_DEFAULT ((uint8_t)0U) |
#define | HWA_FFT_MODE_OUTPUT_MAX_STATS ((uint8_t)2U) |
#define | HWA_FFT_MODE_OUTPUT_SUM_STATS ((uint8_t)3U) |
#define HWA_FFT_MODE_OUTPUT_DEFAULT ((uint8_t)0U) |
Default output (i.e., main data path output is sent out - eg. FFT or Log-Mag output)
#define HWA_FFT_MODE_OUTPUT_MAX_STATS ((uint8_t)2U) |
Statistics output - Max statistics is sent out (Max value on the I arm, Max index on the Q arm)
#define HWA_FFT_MODE_OUTPUT_SUM_STATS ((uint8_t)3U) |
Statistics output - Sum statistics is sent out