Macros that define values for enabling/disabling the magnitude and log2 computation in FFT block.
Macros | |
#define | HWA_FFT_MODE_MAGNITUDE_LOG2_DISABLED ((uint8_t)0U) |
#define | HWA_FFT_MODE_MAGNITUDE_ONLY_ENABLED ((uint8_t)2U) |
#define | HWA_FFT_MODE_MAGNITUDE_LOG2_ENABLED ((uint8_t)3U) |
#define HWA_FFT_MODE_MAGNITUDE_LOG2_DISABLED ((uint8_t)0U) |
magnitude disabled and log2 disabled
#define HWA_FFT_MODE_MAGNITUDE_ONLY_ENABLED ((uint8_t)2U) |
magnitude enabled and log2 disabled
#define HWA_FFT_MODE_MAGNITUDE_LOG2_ENABLED ((uint8_t)3U) |
magnitude and log2 enabled