The section has a list of all the error codes which are generated by the HWA Driver module.
HWA driver Error Codes.
Macros | |
#define | HWA_ERRNO_BASE (-2800) |
HWA driver error base. More... | |
#define | HWA_EINVAL (HWA_ERRNO_BASE-1) |
Error Code: Invalid argument. More... | |
#define | HWA_ENOINIT (HWA_ERRNO_BASE-2) |
Error Code: Operation cannot be done as HWA_init is not done. More... | |
#define | HWA_EOUTOFRANGE (HWA_ERRNO_BASE-3) |
Error Code: input argument out of range. More... | |
#define | HWA_EOUTOFMEM (HWA_ERRNO_BASE-4) |
Error Code: out of memory. More... | |
#define | HWA_ENOTSUPP (HWA_ERRNO_BASE-5) |
Error Code: feature not supported. More... | |
#define | HWA_EINUSE (HWA_ERRNO_BASE-6) |
Error Code: channel or resource in use. More... | |
#define | HWA_ENOTALIGNED (HWA_ERRNO_BASE-7) |
Error Code: address is not aligned to the expected boundary. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_PARAMSET (HWA_ERRNO_BASE-8) |
Error Code: Invalid argument: paramset Start/Stop Idx and numLoops in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_PARAMSET_ALT (HWA_ERRNO_BASE-9) |
Error Code: Invalid argument: paramset Start/Stop Idx and numLoops for context switching in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_FFTCONFIG (HWA_ERRNO_BASE-10) |
Error Code: Invalid argument: for FFT config in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_DCEST (HWA_ERRNO_BASE-11) |
Error Code: Invalid argument: for DC estimation in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_CFAR (HWA_ERRNO_BASE-12) |
Error Code: Invalid argument: for CFAR config in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_INTERFERENCE (HWA_ERRNO_BASE-13) |
Error Code: Invalid argument: for interference localization/mitigation in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_COMPLEXMULT (HWA_ERRNO_BASE-14) |
Error Code: Invalid argument: for complex multiply in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_CHANCOMB (HWA_ERRNO_BASE-15) |
Error Code: Invalid argument: for channel combine in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_ZEROINSERT (HWA_ERRNO_BASE-16) |
Error Code: Invalid argument: for zero insert in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_ADVSTAT (HWA_ERRNO_BASE-17) |
Error Code: Invalid argument: for advanced statistics in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_COMPRESS (HWA_ERRNO_BASE-18) |
Error Code: Invalid argument: for compress/decompression in common register. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_LOCALMAXIMUM (HWA_ERRNO_BASE-19) |
Error Code: Invalid argument: for local maximum in common register. More... | |
#define | HWA_EINVAL_PARAMSET_GENERALCONFIG (HWA_ERRNO_BASE - 20) |
Error Code: Invalid argument: general config in paramset More... | |
#define | HWA_EINVAL_PARAMSET_SOURCE (HWA_ERRNO_BASE - 21) |
Error Code: Invalid argument: source(input formatter) in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_DEST (HWA_ERRNO_BASE - 22) |
Error Code: Invalid argument: destination(output formatter) in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_SRCDST_ADDRESS (HWA_ERRNO_BASE - 23) |
Error Code: Invalid argument: src and dst address in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_FFTMODE_GENERALCONFIG (HWA_ERRNO_BASE - 24) |
Error Code: Invalid argument: FFT mode: general config in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_FFTMODE_SIZE (HWA_ERRNO_BASE - 25) |
Error Code: Invalid argument: FFT mode: FFT size in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_FFTMODE_POSTPROC (HWA_ERRNO_BASE - 26) |
Error Code: Invalid argument: FFT mode: post processing in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_FFTMODE_PREPROC (HWA_ERRNO_BASE - 27) |
Error Code: Invalid argument: FFT mode: pre-processing in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_FFTMODE_PREPROC_INTERF (HWA_ERRNO_BASE - 28) |
Error Code: Invalid argument: FFT mode: pre-processing interference localization/statistics/mitigation in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_FFTMODE_PREPROC_COMPLEXMULT (HWA_ERRNO_BASE - 29) |
Error Code: Invalid argument: FFT mode: pre-processing complex multiply block in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_CFARMODE_GENERALCONFIG (HWA_ERRNO_BASE - 30) |
Error Code: Invalid argument: CFAR mode: general configuration in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_CFARMODE_OSCONFIG (HWA_ERRNO_BASE - 31) |
Error Code: Invalid argument: CFAR mode: CFAR-OS configuration in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_CFARMODE_CACONFIG (HWA_ERRNO_BASE - 32) |
Error Code: Invalid argument: CFAR mode: CFAR-CA configuration in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_COMPRESSMODE (HWA_ERRNO_BASE - 33) |
Error Code: Invalid argument: compress/decompress mode: compress/decompress configuration in paramset. More... | |
#define | HWA_EINVAL_PARAMSET_LOCALMAXMODE (HWA_ERRNO_BASE - 34) |
Error Code: Invalid argument: local maxima mode: local maxima configuration in paramset. More... | |
#define | HWA_PARAMSET_POLLINGNOTALLOWED (HWA_ERRNO_BASE - 35) |
Error Code: if paramset interrupt is enabled, polling should be disabled. More... | |
#define | HWA_EINVAL_COMMON_REGISTER_CFAR_DET_THR (HWA_ERRNO_BASE - 36) |
Error Code: Invalid argument: for CFAR config in common register - CFAR_DET_THR. More... | |
#define HWA_ERRNO_BASE (-2800) |
HWA driver error base.
#define HWA_EINVAL (HWA_ERRNO_BASE-1) |
Error Code: Invalid argument.
#define HWA_ENOINIT (HWA_ERRNO_BASE-2) |
Error Code: Operation cannot be done as HWA_init is not done.
#define HWA_EOUTOFRANGE (HWA_ERRNO_BASE-3) |
Error Code: input argument out of range.
#define HWA_EOUTOFMEM (HWA_ERRNO_BASE-4) |
Error Code: out of memory.
#define HWA_ENOTSUPP (HWA_ERRNO_BASE-5) |
Error Code: feature not supported.
#define HWA_EINUSE (HWA_ERRNO_BASE-6) |
Error Code: channel or resource in use.
#define HWA_ENOTALIGNED (HWA_ERRNO_BASE-7) |
Error Code: address is not aligned to the expected boundary.
#define HWA_EINVAL_COMMON_REGISTER_PARAMSET (HWA_ERRNO_BASE-8) |
Error Code: Invalid argument: paramset Start/Stop Idx and numLoops in common register.
#define HWA_EINVAL_COMMON_REGISTER_PARAMSET_ALT (HWA_ERRNO_BASE-9) |
Error Code: Invalid argument: paramset Start/Stop Idx and numLoops for context switching in common register.
#define HWA_EINVAL_COMMON_REGISTER_FFTCONFIG (HWA_ERRNO_BASE-10) |
Error Code: Invalid argument: for FFT config in common register.
#define HWA_EINVAL_COMMON_REGISTER_DCEST (HWA_ERRNO_BASE-11) |
Error Code: Invalid argument: for DC estimation in common register.
#define HWA_EINVAL_COMMON_REGISTER_CFAR (HWA_ERRNO_BASE-12) |
Error Code: Invalid argument: for CFAR config in common register.
#define HWA_EINVAL_COMMON_REGISTER_INTERFERENCE (HWA_ERRNO_BASE-13) |
Error Code: Invalid argument: for interference localization/mitigation in common register.
#define HWA_EINVAL_COMMON_REGISTER_COMPLEXMULT (HWA_ERRNO_BASE-14) |
Error Code: Invalid argument: for complex multiply in common register.
#define HWA_EINVAL_COMMON_REGISTER_CHANCOMB (HWA_ERRNO_BASE-15) |
Error Code: Invalid argument: for channel combine in common register.
#define HWA_EINVAL_COMMON_REGISTER_ZEROINSERT (HWA_ERRNO_BASE-16) |
Error Code: Invalid argument: for zero insert in common register.
#define HWA_EINVAL_COMMON_REGISTER_ADVSTAT (HWA_ERRNO_BASE-17) |
Error Code: Invalid argument: for advanced statistics in common register.
#define HWA_EINVAL_COMMON_REGISTER_COMPRESS (HWA_ERRNO_BASE-18) |
Error Code: Invalid argument: for compress/decompression in common register.
#define HWA_EINVAL_COMMON_REGISTER_LOCALMAXIMUM (HWA_ERRNO_BASE-19) |
Error Code: Invalid argument: for local maximum in common register.
#define HWA_EINVAL_PARAMSET_GENERALCONFIG (HWA_ERRNO_BASE - 20) |
Error Code: Invalid argument: general config in paramset
#define HWA_EINVAL_PARAMSET_SOURCE (HWA_ERRNO_BASE - 21) |
Error Code: Invalid argument: source(input formatter) in paramset.
#define HWA_EINVAL_PARAMSET_DEST (HWA_ERRNO_BASE - 22) |
Error Code: Invalid argument: destination(output formatter) in paramset.
#define HWA_EINVAL_PARAMSET_SRCDST_ADDRESS (HWA_ERRNO_BASE - 23) |
Error Code: Invalid argument: src and dst address in paramset.
#define HWA_EINVAL_PARAMSET_FFTMODE_GENERALCONFIG (HWA_ERRNO_BASE - 24) |
Error Code: Invalid argument: FFT mode: general config in paramset.
#define HWA_EINVAL_PARAMSET_FFTMODE_SIZE (HWA_ERRNO_BASE - 25) |
Error Code: Invalid argument: FFT mode: FFT size in paramset.
#define HWA_EINVAL_PARAMSET_FFTMODE_POSTPROC (HWA_ERRNO_BASE - 26) |
Error Code: Invalid argument: FFT mode: post processing in paramset.
#define HWA_EINVAL_PARAMSET_FFTMODE_PREPROC (HWA_ERRNO_BASE - 27) |
Error Code: Invalid argument: FFT mode: pre-processing in paramset.
#define HWA_EINVAL_PARAMSET_FFTMODE_PREPROC_INTERF (HWA_ERRNO_BASE - 28) |
Error Code: Invalid argument: FFT mode: pre-processing interference localization/statistics/mitigation in paramset.
#define HWA_EINVAL_PARAMSET_FFTMODE_PREPROC_COMPLEXMULT (HWA_ERRNO_BASE - 29) |
Error Code: Invalid argument: FFT mode: pre-processing complex multiply block in paramset.
#define HWA_EINVAL_PARAMSET_CFARMODE_GENERALCONFIG (HWA_ERRNO_BASE - 30) |
Error Code: Invalid argument: CFAR mode: general configuration in paramset.
#define HWA_EINVAL_PARAMSET_CFARMODE_OSCONFIG (HWA_ERRNO_BASE - 31) |
Error Code: Invalid argument: CFAR mode: CFAR-OS configuration in paramset.
#define HWA_EINVAL_PARAMSET_CFARMODE_CACONFIG (HWA_ERRNO_BASE - 32) |
Error Code: Invalid argument: CFAR mode: CFAR-CA configuration in paramset.
#define HWA_EINVAL_PARAMSET_COMPRESSMODE (HWA_ERRNO_BASE - 33) |
Error Code: Invalid argument: compress/decompress mode: compress/decompress configuration in paramset.
#define HWA_EINVAL_PARAMSET_LOCALMAXMODE (HWA_ERRNO_BASE - 34) |
Error Code: Invalid argument: local maxima mode: local maxima configuration in paramset.
#define HWA_PARAMSET_POLLINGNOTALLOWED (HWA_ERRNO_BASE - 35) |
Error Code: if paramset interrupt is enabled, polling should be disabled.
#define HWA_EINVAL_COMMON_REGISTER_CFAR_DET_THR (HWA_ERRNO_BASE - 36) |
Error Code: Invalid argument: for CFAR config in common register - CFAR_DET_THR.