Macros that define values for the trigger mode of HWA paramsets.
Macros | |
#define | HWA_CONTEXTSWITCH_TRIG_MODE_DMA ((uint8_t)3U) |
#define | HWA_CONTEXTSWITCH_TRIG_MODE_HARDWARE ((uint8_t)4U) |
#define | HWA_CONTEXTSWITCH_TRIG_MODE_SOFTWARE ((uint8_t)5U) |
#define HWA_CONTEXTSWITCH_TRIG_MODE_DMA ((uint8_t)3U) |
state machine reads the paramset but waits for DMA trigger before executing that paramset
#define HWA_CONTEXTSWITCH_TRIG_MODE_HARDWARE ((uint8_t)4U) |
Hardware based trigger #1
#define HWA_CONTEXTSWITCH_TRIG_MODE_SOFTWARE ((uint8_t)5U) |
software trigger