AM273x MCU+ SDK  08.06.00

Introduction

See IPC Notify for more details.

Data Structures

struct  IpcNotify_Params
 Parameters used by IpcNotify_init. More...
 

Functions

void IpcNotify_Params_init (IpcNotify_Params *params)
 Set default value to IpcNotify_Params. More...
 
int32_t IpcNotify_init (const IpcNotify_Params *params)
 Initialize IPC Notify module. More...
 
void IpcNotify_deInit (void)
 De-initialize IPC Notify module. More...
 
int32_t IpcNotify_sendMsg (uint32_t remoteCoreId, uint16_t remoteClientId, uint32_t msgValue, uint32_t waitForFifoNotFull)
 Send message to a specific remote core and specific client ID on that remote core. More...
 
int32_t IpcNotify_registerClient (uint16_t localClientId, IpcNotify_FxnCallback msgCallback, void *args)
 Register a callback to handle messages received from a specific remote core and for a specific local client ID. More...
 
int32_t IpcNotify_unregisterClient (uint16_t localClientId)
 Un-register a previously registered callback. More...
 
uint32_t IpcNotify_getSelfCoreId (void)
 Return current core ID. More...
 
uint32_t IpcNotify_isCoreEnabled (uint32_t coreId)
 Check if a core is enabled for IPC. More...
 
int32_t IpcNotify_sendSync (uint32_t remoteCoreId)
 Send a sync message to specific core. More...
 
int32_t IpcNotify_waitSync (uint32_t remoteCoreId, uint32_t timeout)
 Wait for a sync message to be received from the specified core. More...
 
int32_t IpcNotify_syncAll (uint32_t timeout)
 Send a message to all enabled cores and wait for sync message from all enabled cores. More...
 
void IpcNotify_registerNonNotifyCallback (IpcNotify_NonNotifyCallback callback)
 This is a driver library internal API and is used in certain SOCs by the separate mailbox driver. More...
 

Typedefs

typedef void(* IpcNotify_FxnCallback) (uint32_t remoteCoreId, uint16_t localClientId, uint32_t msgValue, void *args)
 User callback that is invoked when a message is received from a reote core for a given client ID. More...
 
typedef void(* IpcNotify_NonNotifyCallback) (uint32_t remoteCoreId)
 This is a driver library internal API and is used in certain SOCs by the separate mailbox driver. More...
 

Macros

#define IPC_NOTIFY_CLIENT_ID_MAX   (16U)
 Maximum number of clients possible for receiving messages. More...
 
#define IPC_NOTIFY_CLIENT_ID_RPMSG   (0U)
 Client ID used by rpmessage, this client ID should not be used by other users. More...
 
#define IPC_NOTIFY_CLIENT_ID_SYNC   (1U)
 Client ID used for sync messages, this client ID should not be used by other users. More...
 
#define IPC_NOTIFY_MSG_VALUE_MAX   (0x10000000U)
 Maximum value of message that can be sent and received. More...
 

Macro Definition Documentation

◆ IPC_NOTIFY_CLIENT_ID_MAX

#define IPC_NOTIFY_CLIENT_ID_MAX   (16U)

Maximum number of clients possible for receiving messages.

◆ IPC_NOTIFY_CLIENT_ID_RPMSG

#define IPC_NOTIFY_CLIENT_ID_RPMSG   (0U)

Client ID used by rpmessage, this client ID should not be used by other users.

◆ IPC_NOTIFY_CLIENT_ID_SYNC

#define IPC_NOTIFY_CLIENT_ID_SYNC   (1U)

Client ID used for sync messages, this client ID should not be used by other users.

◆ IPC_NOTIFY_MSG_VALUE_MAX

#define IPC_NOTIFY_MSG_VALUE_MAX   (0x10000000U)

Maximum value of message that can be sent and received.

Typedef Documentation

◆ IpcNotify_FxnCallback

typedef void(* IpcNotify_FxnCallback) (uint32_t remoteCoreId, uint16_t localClientId, uint32_t msgValue, void *args)

User callback that is invoked when a message is received from a reote core for a given client ID.

Before invoking the API, the IPC module would have 'popped` the message from the HW or SW FIFO already. This callback is called frm ISR context, so all constraints of ISR should be applied by the callback, e.g. no blocking wait, quickly handle message and exit ISR.

For most applications, it is recommended to put the message value into a local SW queue and defer the message handling itself to a application task.

Parameters
remoteCoreId[in] Remote core that has sent the message
localClientId[in] Local client ID to which the message is sent
msgValue[in] Message value that is sent
args[in] Argument pointer passed by user when IpcNotify_registerClient is called

◆ IpcNotify_NonNotifyCallback

typedef void(* IpcNotify_NonNotifyCallback) (uint32_t remoteCoreId)

This is a driver library internal API and is used in certain SOCs by the separate mailbox driver.

Attention
This API should not be used by end users.
Parameters
remoteCoreId[in] remote core ID that generated the interrupt

Function Documentation

◆ IpcNotify_Params_init()

void IpcNotify_Params_init ( IpcNotify_Params params)

Set default value to IpcNotify_Params.

Parameters
params[out] Default initialized structure

◆ IpcNotify_init()

int32_t IpcNotify_init ( const IpcNotify_Params params)

Initialize IPC Notify module.

This API will initialize the HW used for IPC including registering interrupts for receiving messages.

Parameters
params[in] Initializaion parameters

◆ IpcNotify_deInit()

void IpcNotify_deInit ( void  )

De-initialize IPC Notify module.

This API will de-initialize the HW used for IPC including un-registering interrupts for receiving messages.

◆ IpcNotify_sendMsg()

int32_t IpcNotify_sendMsg ( uint32_t  remoteCoreId,
uint16_t  remoteClientId,
uint32_t  msgValue,
uint32_t  waitForFifoNotFull 
)

Send message to a specific remote core and specific client ID on that remote core.

Note
To reduce latency, error checks are avoided in this API. Users need to make sure the client ID value is < IPC_NOTIFY_CLIENT_ID_MAX and message value is < IPC_NOTIFY_MSG_VALUE_MAX
This API can be called from within ISRs and is also thread-safe. Internally this API disables interrupts for a short while to make the API ISR and thread safe.
One cannot send messages to self, i.e remoteCoreId, cannot be same as core ID of the CPU that called this API.
Parameters
remoteCoreId[in] Remote core to sent message to, see CSL_CoreID for valid values.
remoteClientId[in] Remote core client ID to send message to, MUST be < IPC_NOTIFY_CLIENT_ID_MAX
msgValue[in] Message value to send, MUST be < IPC_NOTIFY_MSG_VALUE_MAX
waitForFifoNotFull[in] 1: wait for message to be inserted into HW or SW FIFO, 0: if FIFO is full, dont send message and return with error.
Returns
SystemP_SUCCESS, message sent successfully
SystemP_FAILURE, message could not be sent since HW or SW FIFO for holding the message is full.

◆ IpcNotify_registerClient()

int32_t IpcNotify_registerClient ( uint16_t  localClientId,
IpcNotify_FxnCallback  msgCallback,
void *  args 
)

Register a callback to handle messages received from a specific remote core and for a specific local client ID.

Parameters
localClientId[in] Client ID to which the message has been sent
msgCallback[in] Callback to invoke, if callback is already registered, error will be returned.
args[in] User arguments, that are passed back to user when the callback is invoked
Returns
SystemP_SUCCESS, callback registered sucessfully
SystemP_FAILURE, callback registration failed, either remoteCoreId or localClientId is invalid or callback already registered.

◆ IpcNotify_unregisterClient()

int32_t IpcNotify_unregisterClient ( uint16_t  localClientId)

Un-register a previously registered callback.

Parameters
localClientId[in] Client ID to which the message has been sent
Returns
SystemP_SUCCESS, callback un-registered sucessfully
SystemP_FAILURE, callback un-registration failed, either remoteCoreId or localClientId is invalid

◆ IpcNotify_getSelfCoreId()

uint32_t IpcNotify_getSelfCoreId ( void  )

Return current core ID.

Returns
Core ID, see CSL_CoreID for valid values.

◆ IpcNotify_isCoreEnabled()

uint32_t IpcNotify_isCoreEnabled ( uint32_t  coreId)

Check if a core is enabled for IPC.

Parameters
coreId[in] Core ID, see CSL_CoreID for valid values.
Returns
1: core is enabled for IPC, 0: core is not enabled for IPC

◆ IpcNotify_sendSync()

int32_t IpcNotify_sendSync ( uint32_t  remoteCoreId)

Send a sync message to specific core.

This API can be used to send sync message's to very specific core's For most users recommend to use the more simpler IpcNotify_syncAll() API.

Parameters
remoteCoreId[in] Core ID, see CSL_CoreID for valid values.
Returns
SystemP_SUCCESS, sync message was sent successfully, else failure

◆ IpcNotify_waitSync()

int32_t IpcNotify_waitSync ( uint32_t  remoteCoreId,
uint32_t  timeout 
)

Wait for a sync message to be received from the specified core.

This API can be used to recevice sync message from very specific core's For most users recommend to use the more simpler IpcNotify_syncAll() API.

Parameters
remoteCoreId[in] Core ID, see CSL_CoreID for valid values.
timeout[in] Amount of time in units of ticks to wait
Returns
SystemP_SUCCESS, sync message was recevied successfully
SystemP_TIMEOUT, sync message was NOT recevied after timeout ticks
SystemP_FAILURE, invalid arguments

◆ IpcNotify_syncAll()

int32_t IpcNotify_syncAll ( uint32_t  timeout)

Send a message to all enabled cores and wait for sync message from all enabled cores.

This API when called on all CPUs, make sure all CPUs execute upto a certain and then proceed only when all other CPUs have also executed to the same point.

This is useful esp during system init to make sure message exchange can be started only after all CPUs have finished their system initialization.

Parameters
timeout[in] Amount of time in units of ticks to wait for the sync
Returns
SystemP_SUCCESS, all sync messages recevied successfully
SystemP_TIMEOUT, some sync messages was NOT recevied after timeout ticks
SystemP_FAILURE, invalid arguments

◆ IpcNotify_registerNonNotifyCallback()

void IpcNotify_registerNonNotifyCallback ( IpcNotify_NonNotifyCallback  callback)

This is a driver library internal API and is used in certain SOCs by the separate mailbox driver.

Attention
This API should not be used by end users.
Parameters
callback[in] Callback to call when a interrupt is received from a CPU which is not part of IPC Notify core list