APIs related to CSIRX D-Phy programming
◆ CSIRX_DphyConfig_init()
Sets default values for configuration.
- Parameters
-
◆ CSIRX_dphySetConfig()
Configure DPHY.
- Parameters
-
handle | [in] CSIRX driver handle |
config | [in] DPHY configuration |
- Returns
- SystemP_SUCCESS on success, else failure
◆ CSIRX_dphyIsControlClockResetDone()
int32_t CSIRX_dphyIsControlClockResetDone |
( |
CSIRX_Handle |
handle, |
|
|
bool * |
isDone |
|
) |
| |
Check if DPHY control clock reset is done.
- Parameters
-
handle | [in] CSIRX driver handle |
isDone | [out] true: reset is done, false: reset is not done |
- Returns
- SystemP_SUCCESS on success, else failure
◆ CSIRX_dphyIsByteClockResetDone()
int32_t CSIRX_dphyIsByteClockResetDone |
( |
CSIRX_Handle |
handle, |
|
|
bool * |
isDone |
|
) |
| |
Check if DPHY byte clock reset is done.
- Parameters
-
handle | [in] CSIRX driver handle |
isDone | [out] true: reset is done, false: reset is not done |
- Returns
- SystemP_SUCCESS on success, else failure
◆ CSIRX_dphyIsClockMissingDetectorError()
int32_t CSIRX_dphyIsClockMissingDetectorError |
( |
CSIRX_Handle |
handle, |
|
|
bool * |
isError |
|
) |
| |
Check if DPHY clock missing detector error.
This API is only meaningful if CSIRX_DphyConfig::isClockMissingDetectionEnabled was configured to true i.e clock missing detector was enabled.
- Parameters
-
handle | [in] CSIRX driver handle |
isError | [out] true: error is detected, false: no error |
- Returns
- SystemP_SUCCESS on success, else failure