AM273x MCU+ SDK  08.06.00
CBUFF Driver External Functions

Introduction

The section has a list of all the exported API which the applications need to invoke in order to use the driver.

Functions

void CBUFF_init (void)
 Description
This function initializes the CBUFF module. This function must be called before any other functions are called. More...
 
CBUFF_Handle CBUFF_open (CBUFF_InitCfg *ptrInitCfg, int32_t *errCode)
 Description
The function Configures CBUFF peripheral with user provided configuration. More...
 
CBUFF_SessionHandle CBUFF_createSession (CBUFF_Handle cbuffHandle, CBUFF_SessionCfg *ptrSessionCfg, int32_t *errCode)
 Description
The function creates a session with the specified configuration. More...
 
int32_t CBUFF_close (CBUFF_SessionHandle sessionHandle, int32_t *errCode)
 Description
The function deletes the specific session. More...
 
int32_t CBUFF_deinit (CBUFF_Handle cBuffHandle, int32_t *errCode)
 Description
The function is used to deinitialize and shutdown the CBUFF driver. More...
 
int32_t CBUFF_control (CBUFF_Handle cBuffHandle, CBUFF_Command cmd, void *arg, uint32_t argLen, int32_t *errCode)
 Description
The function is used to get/set information from the CBUFF Driver. More...
 
int32_t CBUFF_activateSession (CBUFF_SessionHandle sessionHandle, int32_t *errCode)
 Description
The function activates the specific CBUFF session. More...
 
int32_t CBUFF_deactivateSession (CBUFF_SessionHandle sessionHandle, int32_t *errCode)
 Description
The function deactivates the specific CBUFF session. More...
 

Function Documentation

◆ CBUFF_init()

void CBUFF_init ( void  )

Description
This function initializes the CBUFF module. This function must be called before any other functions are called.

◆ CBUFF_open()

CBUFF_Handle CBUFF_open ( CBUFF_InitCfg ptrInitCfg,
int32_t *  errCode 
)

Description
The function Configures CBUFF peripheral with user provided configuration.

Parameters
[in]ptrInitCfgA pointer to CBUFF_InitCfg structure for initialization
[out]errCodePointer to an error code populated by the driver.
Returns
Success - Handle to the CBUFF Driver Error - NULL

◆ CBUFF_createSession()

CBUFF_SessionHandle CBUFF_createSession ( CBUFF_Handle  cbuffHandle,
CBUFF_SessionCfg ptrSessionCfg,
int32_t *  errCode 
)

Description
The function creates a session with the specified configuration.

Parameters
[in]cbuffHandleHandle to the CBUFF driver.
[in]ptrSessionCfgPointer to the session configuration.
[out]errCodePointer to an error code populated by the driver.
Returns
Success - Handle to the session Error - NULL

◆ CBUFF_close()

int32_t CBUFF_close ( CBUFF_SessionHandle  sessionHandle,
int32_t *  errCode 
)

Description
The function deletes the specific session.

Parameters
[in]sessionHandleHandle to the CBUFF session.
[out]errCodePointer to an error code populated by the driver.
Returns
Success - CBUFF_STATUS_SUCCESS Error - CBUFF_ERROR_CODES

◆ CBUFF_deinit()

int32_t CBUFF_deinit ( CBUFF_Handle  cBuffHandle,
int32_t *  errCode 
)

Description
The function is used to deinitialize and shutdown the CBUFF driver.

Parameters
[in]cBuffHandleHandle to the CBUFF instance obtained through call to CBUFF_open.
[out]errCodePointer to an error code populated by the driver.
Returns
Success - CBUFF_STATUS_SUCCESS Error - CBUFF_ERROR_CODES

◆ CBUFF_control()

int32_t CBUFF_control ( CBUFF_Handle  cBuffHandle,
CBUFF_Command  cmd,
void *  arg,
uint32_t  argLen,
int32_t *  errCode 
)

Description
The function is used to get/set information from the CBUFF Driver.

Parameters
[in]cBuffHandleHandle to the CBUFF instance obtained through call to CBUFF_open.
[in]cmdCBUFF command
[in]argCommand specified pointer to the argument
[in]argLenLength of the argument
[out]errCodePointer to an error code populated by the driver.
Returns
Success - CBUFF_STATUS_SUCCESS Error - CBUFF_ERROR_CODES

◆ CBUFF_activateSession()

int32_t CBUFF_activateSession ( CBUFF_SessionHandle  sessionHandle,
int32_t *  errCode 
)

Description
The function activates the specific CBUFF session.

Parameters
[in]sessionHandleHandle to the session to be activated CBUFF_createSession.
[out]errCodePointer to an error code populated by the driver.
Returns
Success - CBUFF_STATUS_SUCCESS Error - CBUFF_ERROR_CODES

◆ CBUFF_deactivateSession()

int32_t CBUFF_deactivateSession ( CBUFF_SessionHandle  sessionHandle,
int32_t *  errCode 
)

Description
The function deactivates the specific CBUFF session.

Parameters
[in]sessionHandleHandle to the session to be deactivated CBUFF_createSession.
[out]errCodePointer to an error code populated by the driver.
Returns
Success - CBUFF_STATUS_SUCCESS Error - CBUFF_ERROR_CODES