EDMA Parameter RAM Set in User Configurable format This is a mapping of the EDMA PaRAM set provided to the user for ease of modification of the individual fields.
Structure containing parameters for STC module configuration.
Data Fields | |
uint32_t | opt |
uint32_t | srcAddr |
Starting byte address of Source For FIFO mode, srcAddr must be a 256-bit aligned address. More... | |
uint16_t | aCnt |
uint16_t | bCnt |
uint32_t | destAddr |
Starting byte address of destination For FIFO mode, destAddr must be a 256-bit aligned address. i.e. 5 LSBs should be 0. More... | |
int16_t | srcBIdx |
Index between consec. arrays of a Source Frame (SRCBIDX). SRCBIDX is 24 Bit field. Lower 16 Bits are stored in this field. Higher 8 Bits are stored in srcBIdxExt. More... | |
int16_t | destBIdx |
Index between consec. arrays of a Destination Frame (DSTBIDX). DSTBIDX is 24 Bit field. Lower 16 Bits are stored in this field. Higher 8 Bits are stored in destBIdxExt. More... | |
uint16_t | linkAddr |
Address for linking (AutoReloading of a PaRAM Set) This must point to a valid aligned 32-byte PaRAM set A value of 0xFFFF means no linking. More... | |
uint16_t | bCntReload |
Reload value of the numArrInFrame (BCNT) Relevant only for A-sync transfers. More... | |
int16_t | srcCIdx |
int16_t | destCIdx |
uint16_t | cCnt |
int8_t | srcBIdxExt |
int8_t | destBIdxExt |
uint32_t | lpScanMode |
uint32_t | codecSpreadMode |
uint32_t | capIdleCycle |
uint32_t | scanEnHighCap_idleCycle |
uint32_t | intervalNum |
uint32_t | maxRunTime |
uint32_t | clkDiv |
uint32_t | romStartAddress |
uint32_t | pRomStartAdd |
uint32_t | faultInsert |
uint32_t | stcDiagnostic |
SDL_STC_ScanModeconfig | modeConfig |
uint32_t __attribute__::opt |
uint32_t __attribute__::srcAddr |
Starting byte address of Source For FIFO mode, srcAddr must be a 256-bit aligned address.
uint16_t __attribute__::aCnt |
uint16_t __attribute__::bCnt |
uint32_t __attribute__::destAddr |
Starting byte address of destination For FIFO mode, destAddr must be a 256-bit aligned address. i.e. 5 LSBs should be 0.
int16_t __attribute__::srcBIdx |
Index between consec. arrays of a Source Frame (SRCBIDX). SRCBIDX is 24 Bit field. Lower 16 Bits are stored in this field. Higher 8 Bits are stored in srcBIdxExt.
int16_t __attribute__::destBIdx |
Index between consec. arrays of a Destination Frame (DSTBIDX). DSTBIDX is 24 Bit field. Lower 16 Bits are stored in this field. Higher 8 Bits are stored in destBIdxExt.
uint16_t __attribute__::linkAddr |
Address for linking (AutoReloading of a PaRAM Set) This must point to a valid aligned 32-byte PaRAM set A value of 0xFFFF means no linking.
uint16_t __attribute__::bCntReload |
Reload value of the numArrInFrame (BCNT) Relevant only for A-sync transfers.
int16_t __attribute__::srcCIdx |
int16_t __attribute__::destCIdx |
uint16_t __attribute__::cCnt |
int8_t __attribute__::srcBIdxExt |
int8_t __attribute__::destBIdxExt |
uint32_t __attribute__::lpScanMode |
Scan mode configuration. Fixed Configuration – Only this configuration value is supported.
uint32_t __attribute__::codecSpreadMode |
Scan mode configuration. Fixed Configuration – Only this configuration value is supported
uint32_t __attribute__::capIdleCycle |
Scan mode configuration. Fixed Configuration – Only this configuration value is supported
uint32_t __attribute__::scanEnHighCap_idleCycle |
Scan mode configuration. Fixed Configuration – Only this configuration value is supported
uint32_t __attribute__::intervalNum |
Configure number of intervals
uint32_t __attribute__::maxRunTime |
Max run time for STC
uint32_t __attribute__::clkDiv |
Clock division value for STC clock
uint32_t __attribute__::romStartAddress |
Configure Rom start address
uint32_t __attribute__::pRomStartAdd |
Pointer of Rom start address
uint32_t __attribute__::faultInsert |
Configure this for insert fault in STC test vector
uint32_t __attribute__::stcDiagnostic |
Configure this for enabling STC diagnostic check
SDL_STC_ScanModeconfig __attribute__::modeConfig |
Configure scan mode configuration