AM273x MCU+ SDK  08.05.00
MCASP_EdmaConfig Struct Reference

Detailed Description

MCASP edma configuration object.

Data Fields

uint32_t baseAddr
 
uint32_t regionId
 
uint32_t chId
 
uint32_t paramId
 
uint32_t tccId
 
uint32_t linkParamId
 
Edma_IntrObject intrObj
 

Field Documentation

◆ baseAddr

uint32_t MCASP_EdmaConfig::baseAddr

EDMA instance base address

◆ regionId

uint32_t MCASP_EdmaConfig::regionId

EDMA region Id

◆ chId

uint32_t MCASP_EdmaConfig::chId

DMA Channel Number. This should be the MCASP Event number

◆ paramId

uint32_t MCASP_EdmaConfig::paramId

EDMA parameter ram Id

◆ tccId

uint32_t MCASP_EdmaConfig::tccId

EDMA transfer completion code

◆ linkParamId

uint32_t MCASP_EdmaConfig::linkParamId

EDMA link parameter ram Id

◆ intrObj

Edma_IntrObject MCASP_EdmaConfig::intrObj