AM273x MCU+ SDK  08.05.00

Detailed Description

Input args for CPSW_ALE_IOCTL_GET_PORT_MACADDR command.

Data Fields

uint32_t portNum
 
CpswAle_MacAddrInfoaddrs
 
uint32_t addrCnt
 

Field Documentation

◆ portNum

uint32_t CpswAle_GetPortMacAddrInArgs::portNum

Port number for which MAC addresses are being queried

◆ addrs

CpswAle_MacAddrInfo* CpswAle_GetPortMacAddrInArgs::addrs

Application provided buffer into which MAC addresses will be populated

◆ addrCnt

uint32_t CpswAle_GetPortMacAddrInArgs::addrCnt

Max number of MAC entries that can be stored in provided buffer