AM273x MCU+ SDK  08.05.00

Detailed Description

DPHY configuration.

Data Fields

uint32_t ddrClockInHz
 DDR clock speed in Hz. More...
 
bool isClockMissingDetectionEnabled
 Set to true if wanting to enable clock missing detector. More...
 
uint8_t triggerEscapeCode [4]
 Trigger escape codes. More...
 

Field Documentation

◆ ddrClockInHz

uint32_t CSIRX_DphyConfig::ddrClockInHz

DDR clock speed in Hz.

◆ isClockMissingDetectionEnabled

bool CSIRX_DphyConfig::isClockMissingDetectionEnabled

Set to true if wanting to enable clock missing detector.

◆ triggerEscapeCode

uint8_t CSIRX_DphyConfig::triggerEscapeCode[4]

Trigger escape codes.