AM273x MCU+ SDK  08.05.00
CSIRX_ContextCropConfig Struct Reference

Detailed Description

Cropping configuration.

Data Fields

uint16_t horizontalCount
 13-bit field that indicates pixels to output per line when value is between 1 and 8191. Pixels horizontalSkip - (image width provided by sensor) are output when this value is 0. More...
 
uint16_t horizontalSkip
 Pixels to skip horizontally between 0 and 8191. More...
 
uint16_t verticalCount
 13-bit field that indicates lines to output per frame when value is between 1 and 8191. Pixels verticalSkip - (image height provided by sensor) are output when this value is 0. More...
 
uint16_t verticalSkip
 Pixels to skip vertically between 0 and 8191. More...
 

Field Documentation

◆ horizontalCount

uint16_t CSIRX_ContextCropConfig::horizontalCount

13-bit field that indicates pixels to output per line when value is between 1 and 8191. Pixels horizontalSkip - (image width provided by sensor) are output when this value is 0.

◆ horizontalSkip

uint16_t CSIRX_ContextCropConfig::horizontalSkip

Pixels to skip horizontally between 0 and 8191.

◆ verticalCount

uint16_t CSIRX_ContextCropConfig::verticalCount

13-bit field that indicates lines to output per frame when value is between 1 and 8191. Pixels verticalSkip - (image height provided by sensor) are output when this value is 0.

◆ verticalSkip

uint16_t CSIRX_ContextCropConfig::verticalSkip

Pixels to skip vertically between 0 and 8191.